STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

incrementation of a timer by an input signal

Posted on May 09, 2012 at 17:18hi, i'm trying ton increment a timer in timing mode at each rising of a signal which arrive on an other pin here my code :     RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2,ENABLE);     RCC_APB1PeriphClockCmd(RCC_APB1Pe...

claire by Associate III
  • 2140 Views
  • 5 replies
  • 0 kudos

I2S/SPI interrupts

Posted on May 10, 2012 at 17:07Hi, I am using STM32F105RB and I have a problem with an I2S master receive connection, using SPI2. I have configured SPI2 in I2S master Receiver mode, and enabled a SPI2 receive interrupt but immediately after SPI2 ini...

0-wait state

Posted on May 10, 2012 at 15:19Hello, I am evaluating the SMT32F407 and I am wondering how it is possible to execute code from flash with 0-wait state. In the datasheet on page 67 it is described that the number of wait states it 5 at the maximum C...

STM32L152 TIM5

Posted on May 10, 2012 at 11:17I have an interesting problem I hope someone can explain.I was trying to modify the PWM_Input example from the StdPeriph examples to work with TIM5 so I could get a longer range. I have tried to use both TIM5_CH2 (PA1)...

problem read input data

Posted on May 10, 2012 at 14:12i am on the stm32l discovery and i send a square wave on the pin PA1 but it's like i don't receive it, i'm trying to read it with the function GPIO_ReadInputDataBit(GPIOA, GPIO_Pin_1) but it desn't work !! int main(voi...

claire by Associate III
  • 1398 Views
  • 2 replies
  • 0 kudos

5.7'' TFT display 640X480 16bit FSMC part number

Posted on May 08, 2012 at 12:08For my current project we are using a development board of powerAVR. It has a 3.5� TFT touchpanel with resolution 320x240, using 16bit FSMC bus for communication. But I need to have implement it on a 5.7� TFT with ...

sri1904 by Associate
  • 1699 Views
  • 3 replies
  • 0 kudos

STM32F207 IOs output voltage levels

Posted on May 09, 2012 at 14:37Hi all,I need some information regarding the STM32F207 IOs output voltage levels... in fact according to the datasheet (Table 44) the VOH Min is:- 2.4 V for CMOS ports- VDD - 0,4 for TTL port.However I know that all ST...

CAN interrupts does not work

Posted on May 08, 2012 at 10:13 hello everyone! Help me, please, to find where is a bug in my programm for CAN slave. I have two boards. One is evaluation sk-mstm32f It sends requests. And the other board is my own board on stm32f103, which ...

std peripheral library error on stm32f207ve

Posted on May 10, 2012 at 01:17This function:  ITStatus DMA_GetITStatus(DMA_Stream_TypeDef* DMAy_Streamx, uint32_t DMA_IT);Does not correctly detect the interrupt status on this chip.   The interrupt status can be correctly discovered by the simple ...

bruce2399 by Associate II
  • 1137 Views
  • 1 replies
  • 0 kudos