User Activity

For a 21-channel temperature measurement tool (NTCs) I use a STM32F373 ( SDADC1 + SDADC2 + SDADC3). I replaced a temperature sensor with a fixed resistor for these tests.The behavior of the ADCs is different and reproducible after startup:Good Case: ...
Posted on September 23, 2013 at 08:42I�ve have a problem with the ADCs in dual regular simultaneous mode. I want to measure 3 channels with ADC1 and 3 channels with ADC2. The conversions are started by software. I want to get 32 acquisitions in DMA ...
Posted on July 03, 2013 at 14:49I have a STM32F107VC-SK IAR demo board and I want to implment the Micrium uC / TCP-IP stack. What are the changes in the BSP? #stm32-tcp
Posted on July 21, 2010 at 13:51 TIM4 and CAN on PB
Posted on July 19, 2010 at 13:25 TIM4 PWM Out