STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem with send function in USART1 - STM32VL Discovery

Posted on July 05, 2012 at 01:52Hello.I'm facing a problem when trying to send data with function USART_SendData(USART1, (uint16_t)resultat) (resultat is a int 32 bits).When i step by step debugged it, i discovered that my program just enters in an ...

favero by Associate
  • 1498 Views
  • 3 replies
  • 0 kudos

Error fsmc stm32f4discovery

Posted on July 01, 2012 at 13:32 Hi, everyone. I'm testing on fsmc stm32f407VG. I use the Address / Data multiplexed on databus (MUXEN = 1). 2 modes of testing EXTMOD = 0 and 1. Initialization:  FSMC_Bank1->BTCR[0] = //FSMC_BCR2_EXTMOD |           ...

sergej by Associate II
  • 2154 Views
  • 3 replies
  • 0 kudos

Real-time command execution STM32F407

Posted on July 01, 2012 at 13:57Hi, everyone. Testing STM32F407. Runs it at 168 MHz (5.92 ns cycle), FLASH-> ACR = FLASH_ACR_DCEN | FLASH_ACR_ICEN | FLASH_ACR_PRFTEN | FLASH_ACR_LATENCY_5WS. Outstanding at the PA1 a simple square wave:  PM_(RCC->AHB...

sergej by Associate II
  • 3826 Views
  • 5 replies
  • 0 kudos

Ethernet to serial.

Posted on July 04, 2012 at 10:38Hi,i have IAR KickStart Kit for STM32F107VC and i use some code for Ethernet and its running well, it can send the UDP packet and receive it, now i want to see the recived packet so i am trying to send all the incomin...

hello by Associate II
  • 3621 Views
  • 7 replies
  • 0 kudos

value at fixed memory address

Posted on July 03, 2012 at 08:32hi i want to place value - ''address of station'' at fixed memory address without specifed address its look like &sharpdefine mcu_address 0x03 i found - it may looks like &sharpdefine mcu_address         (*((volati...

redkofka by Associate II
  • 1808 Views
  • 3 replies
  • 0 kudos

Non interrupt driven ms timer

Posted on July 03, 2012 at 09:43Hi,I'm currently trying to implement a non interrupt driven millisecond timer. I have alot of other interrupts and functions, which i do not want to interrupt to increment a timer value. Also, i've already implemented...

thommagn by Associate II
  • 2037 Views
  • 4 replies
  • 0 kudos

STM32 & ethernet & board

Posted on June 29, 2012 at 10:23Hi. I have a STM32f3220g-eval board.  I tried  lwip standalone stack. It doesn't work, I made same in the document UM1057. Jumpers and selecting modes from software are ok. Dhcp or pinging response does not work Also ...

biralti by Associate II
  • 2691 Views
  • 5 replies
  • 0 kudos

GPIO specs for the STM32F0 parts

Posted on July 02, 2012 at 06:31Hi all, I need to know more about the GPIO current source / sinking  capabilities of the STM32F0 family. According to Table 18 in the STM32F051C8 datasheet (DM00039193.pdf) the maximum current that can be sinked/sourc...

halherta2 by Associate II
  • 2063 Views
  • 3 replies
  • 0 kudos

STM32F107 CRC not working...

Posted on June 26, 2012 at 00:29Hi all, I'm trying to use the CRC module in a STM32F107 using IAR EW and I'm not getting very far. I'm using the standard stm32f10x_crc.c library but looking in the debugger, any writes to CRC_DR or CRC_CR are being i...

stforum23 by Associate II
  • 1716 Views
  • 4 replies
  • 0 kudos

Question About USB device Lib

Posted on June 24, 2012 at 14:23Hello I'm working on USB device library V3.3.0; I'm new be in STM32 USB; I have some question:could you please help me 1/ I don't understand why SYSCFG module clock is used for the USB disconnect feature ? 2/ What GP...

gafsos by Associate II
  • 1436 Views
  • 3 replies
  • 0 kudos