STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Double Buffering In USB device LIB V3.3

Posted on July 10, 2012 at 14:48Hello, i have a question regarding USB Bulk Example (Mass Stoarge) in ST USB device Lib V3.3 Does someone know if double buffering is activated in these example codes, i think it is not activated.How can i activate it...

gafsos by Associate II
  • 692 Views
  • 0 replies
  • 0 kudos

uart interrupt problem

Posted on July 06, 2012 at 16:52The original post was too long to process during our migration. Please click on the attachment to read the original post.

vinothraj by Associate II
  • 2982 Views
  • 6 replies
  • 0 kudos

stm32w Contiki

Posted on January 17, 2012 at 07:32Hello,I load Contiki 2.5 to mb851 and it works well,but in my own board (with the same chip stm32w108CBU63) radio library not works.In IAR simplemac-library works fine.Does anybody know why?Thank you. #stm32w108

radomir by Associate II
  • 2635 Views
  • 6 replies
  • 0 kudos

Trouble writing STP1612PW05 config

Posted on July 06, 2012 at 22:27Please note that I'm not using an ST microprocessor or controller, but I am using the STP1612PW05.  I am having extreme difficulty finding support on this chip.  I can't find any more appropriate a forum than this one...

I²C read operation freezing

Posted on June 15, 2012 at 18:08Hello guys, I've got the following problem: I'm trying to read a register of a gyroscope with I²C. Everything works fine as long as I'm using several delays during the I²C communication. This wasn't a problem until ...

wolfram2 by Associate II
  • 4511 Views
  • 12 replies
  • 0 kudos

EXTI interupt not firing. Setup issue?

Posted on January 31, 2012 at 22:53 Here is my code block for setting up the EXTI for Port B pin 0: void VFD_Busy_EXTI_Init( void ){ GPIO_InitTypeDef GPIO_InitStructure; EXTI_InitTypeDef EXTI_InitStructure; NVIC_InitTypeDef NVIC_InitS...

shannon2 by Associate II
  • 1753 Views
  • 6 replies
  • 0 kudos

DAC output buffer - DC offset

Posted on July 04, 2012 at 21:33Hallo, I have not found, in the stm32f100x reference manual or data sheet, any mentioning of a DC offset on the DAC. But if use DAC_OutputBuffer_Enable, I get ~ 60 mV on the pins (nothing connected but a scope) when c...

ST-Link utility doesn't program a byte at the end of memory

Posted on July 03, 2012 at 09:55I've just purchased ST-Link/2 programmer and installed ST-Link Utility v.2.3.0. I load intel hex file which contains 0x55, 0xAA at adressess 0x0800FFFE and 0x0800FFFF respectively. The device is STM32F103C8T6.  Howeve...

kekon1234 by Associate III
  • 2693 Views
  • 4 replies
  • 0 kudos