cancel
Showing results for 
Search instead for 
Did you mean: 

STOP mode and BOOT0 pin

danilo239955
Associate II
Posted on April 14, 2011 at 14:33

STOP mode and BOOT0 pin

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
John F.
Senior
Posted on May 17, 2011 at 14:31

I agree that beyond specifying BOOT0 as an INPUT, there's no other technical information. I would guess that the pin is a genuine floating input without pull up or pull down as these are associated with Input / Output pins. Also, where ST have used integrated resistors as on the JTAG pins they have documented it.

Why not submit a Technical Support query and report back the answer here?

domen23
Associate II
Posted on May 17, 2011 at 14:31

It's floating input.

We have it pulled to ground, and in STOP mode we consume around 30uA.
danilo239955
Associate II
Posted on May 17, 2011 at 14:31

Hi Domen,

thank you for your response.