STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

chose good compiler

Posted on October 14, 2012 at 22:46Hi allI started program the stm32f4 with atollic true studio one month ago it's very good and powerful but right now i have problem with code size limit . I want to know is there any free compiler for stm32f4 ? I l...

imanpakii by Associate III
  • 4303 Views
  • 9 replies
  • 0 kudos

Connected USB device not detected

Posted on October 22, 2012 at 14:52Hello! I have implemented the USB MSC Host application on a STM32F4, but it never detects the connected USB stick in the USBH_core state machine. I also know that the OTG_FS_IRQHandler() never gets executed the who...

reading processor VRefInt voltage

Posted on October 22, 2012 at 11:39I want to measure ADCx_IN17 (internally connected to processor VRefInt). What sample time should I use ?

wadi by Associate II
  • 1797 Views
  • 3 replies
  • 0 kudos

UART4 Interrupt

Posted on October 22, 2012 at 03:45Hello, I am working on STM32F4Discovery Board. I am trying to make the UART4 connection with interrupt. I have declared all the needed settings but not able to find the problem. The problem is that it doesn't go t...

Programming,

Posted on October 21, 2012 at 19:43I have a problem with programming a Stm32f0Discovery board,When i have a code built and the board connected with STM32 ST-LINK Utility, and i click program it says: No Stlink detected.What am i doing wrong,

High Speed IO?? Is it really true?

Posted on October 22, 2012 at 13:20Hi all,I bougth a STM32F2 evulation board and iam trying to use high speed IO's but i didnt succes. here is the code;RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOF, ENABLE);  /* Configure PG6 and PG8 in output pushpul...

himmet by Associate
  • 1243 Views
  • 1 replies
  • 0 kudos

STM32 RC5 STOP MODE ???

Posted on August 06, 2011 at 02:56I want to use low power mode (STOP). i put two configurations here... In the first configuration i am putting 2 STOP mode but first runs... When i wait the same external interrupt despite i enable this, i cant run b...

irmakci by Associate II
  • 1680 Views
  • 3 replies
  • 0 kudos

Circular DMA does not circle for ADC (STM32L1xx)

Posted on October 19, 2012 at 17:49I'm trying to use the ADC on an STM32L1xx to read a single channel with a sample rate based on TIM2.  I plan to use a double-buffering scheme, so I want to set it up to DMA into a buffer with half-complete and full...

stmburns by Associate II
  • 1805 Views
  • 4 replies
  • 0 kudos

1 external RAM shared between 2 separate FSMCs

Posted on October 16, 2012 at 17:14Hi all, I'd like to make 2 STM32F407 share 1 external RAM as a common memory. Chip #1 would store some data in RAM for chip #2, then stop all accesses and signal to #2 that there is some data for him. Chip #2 would...

dmakhrov9 by Associate II
  • 5989 Views
  • 17 replies
  • 0 kudos