STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Simultaneous DMAs: Poor docs or restrictive hardware?

Posted on October 19, 2012 at 18:51The STM32L1xx reference manual has this text in the DMA section: The 7 requests from the peripherals (TIMx[2,3,4,6,7], ADC1, SPI[1,2], I2Cx[1,2], USARTx[1,2,3]) and DAC Channelx[1,2] are simply logically ORed...

stmburns by Associate II
  • 1357 Views
  • 2 replies
  • 0 kudos

sysTick stops after a few TIM3 interrupts

Posted on October 19, 2012 at 16:47Hello, I am having problems with the syStick timer.  The handler for sysTick stops being called after one or two interrupts from TIM3 (set < 1Hz). The TIM3 interrupt has no problem (LED keeps toggling). I started ...

SPI Clock Frequency

Posted on October 18, 2012 at 17:56Hi,I'm having a bit of trouble configuring the SPI2 clock frequency on an STM32F407VG, or perhaps I am confused as to how it works.Using a 25Mhz external oscillator, boosting up to system clock frequency of 168MHz....

bpentz by Associate II
  • 2759 Views
  • 3 replies
  • 0 kudos

SPI Code Help

Posted on October 19, 2012 at 10:18Hello All,  I am using STM32Fs series and I am writing a code for SPI2 . I have to read and write from the slave device. I have to read the data when RX buffer is full and write data continuoulsy to another device....

STM32F4 Usart1 problem

Posted on October 18, 2012 at 11:01 Hi, Im using a STM32f405RG and i am trying to get a simple USART example to work. I load the following code to the mcu: #include ''stm32f4xx.h'' #include ''stm32f4xx_gpio.h'' #include ''st...

thommagn by Associate II
  • 3162 Views
  • 7 replies
  • 0 kudos

how to get complementary output at timer CH1 and CH1N ?

Posted on October 16, 2012 at 18:50hello forum,    the processor is STM32F103    I have an H bridge for DC motor   I want complementary outputs of CH1 and CH1N  I setup the timer 1 as following     TIM_TimeBaseStructure.TIM_Prescaler = 0;   TIM_Tim...

Literal error in stm32f10x.h?

Posted on October 18, 2012 at 11:15In STM32F10x Standart Peripherals Library v3.5.0, stm32f10x.h, line 3616:&sharpdefine  DMA_CCR7_PSIZE            ,         ((uint16_t)0x0300)Not needed comma? #stm32f10x-spl #error

frequencies of STM32F4

Posted on October 17, 2012 at 11:48Hi everyone!I'm new to the world of microcontrollers, these days I'm doing my first espeienze with STM324 discovery, I'm reading the various manuals and trying out the various examples, but I can not understand how...

betuel by Associate II
  • 1979 Views
  • 3 replies
  • 0 kudos

Disabling_SysTick timer

Posted on October 18, 2012 at 08:59Hi everybody. I used SysTick timer as a counter of time in my application throug using of interruption. I found ''SysTick_Config'' function in core_cm0.h file. This function load time to reload register and switch ...

32kHz resonator with 12.5 pF - what will happen ?

Posted on October 17, 2012 at 11:38Due to an error in manufacturing we have a lot of modules with a 32khz resonator with 12.5 pF for low speed external clock and two 27pF aditional capacitor to ground. Prozessor is the STM32F103RCT6. The real time ...

colsman by Associate II
  • 1858 Views
  • 4 replies
  • 0 kudos