cancel
Showing results for 
Search instead for 
Did you mean: 

STM32f100: empty project for IAR Embedded Workbench

Posted on June 21, 2011 at 18:21

Hi, I have to create a firmware using stm32f100 microcontroller.

I don't be able to start because the project that i use doesn't function.

I need someone that is working, or he has morked whit this micro and with this program and can send me the project file structure by email.

I would use the STM32F10x_StdPeriph_Lib_V3.5.0.

Thank you!!

#microcontroller-projects #firmware-library #stm32
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on June 21, 2011 at 18:55

The VL-Discovery board uses the STM32F100

At least as of V3.3 which I have to hand, the firmware packages have empty templates for assorted IDE's, and some pretty vacant projects too for that matter.

Suggest to duplicate one of those, and trim it to your requirements.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on June 21, 2011 at 22:51

good advise, thank you.

But i'd like to found something about stm32f100r4 (it has less ram and less flash.  

http://www.st.com/internet/mcu/product/216841.jsp

)..i don't think the project settin is the same for the two microcontroller. If someone know something about stm32f100r4 i will happy.

Anyway it's a good point to start!