Quick STREX question
Posted on February 08, 2013 at 17:34 Hi, I have a quick quiestion: my toolchain complains that instruction strexb r2, r2, [r3] is illegal (registers may not be the same), while strex r2, r2, [r0] is fine. The qu...
Ask questions, find answers, and share insights on STM32 products and their technical features.
Posted on February 08, 2013 at 17:34 Hi, I have a quick quiestion: my toolchain complains that instruction strexb r2, r2, [r3] is illegal (registers may not be the same), while strex r2, r2, [r0] is fine. The qu...
Posted on February 06, 2013 at 15:43Im using a quadrature encoder hooked up to TIM3-CH1/2 and it works fine, counting both edges, up and down. First question is how to read the TIM3-counter values from within a regular (50 us) ISR. Using TIM_GetCoun...
Posted on February 08, 2013 at 14:22In pal.h{............................................typedef enum { PAL_IOLSTATE_NOREQUEST, PAL_IOLSTATE_ACTIVE_REQUEST, PAL_IOLSTATE_APP_ACTIVE} pal_RequestState_t;extern pal_RequestState_t pal_eReques...
Posted on February 06, 2013 at 13:31 hello, i'm trying to connect my stm32f0 discovery with the pc and set up a uart connection. I have found the following code (in this community) but i can't get it to work. Does anyone have a suggestion...
Posted on February 04, 2013 at 04:05It appears the TIM4 OC interrupts on CH2 results in occasionally missing an Update (overflow) interrupt. The situation is a 1 PPS GPS pulse triggers the TIM4 CH1 input capture. The 16 bit counter time is extend...
Posted on February 08, 2013 at 00:09Hello everyone. A week ago, I fought with a STM32F103, trying to get it fill some random buffer with its DMA1_Channel1 controller from its USART1 Rx ''events''. But neither the recipient memory would get filled, ...
Posted on February 05, 2013 at 14:06The original post was too long to process during our migration. Please click on the attachment to read the original post.
Posted on February 07, 2013 at 05:12I am trying to send data to a PC COM port but cannot figure it outI configured GPIO, NVIC, and USART per specification and it all checks out. The strange thing is, when I connect the Tx pin and ground to oscillosc...
Posted on February 07, 2013 at 13:22Hi ,I have two development board which is the first have stm32f103vg LQFP100and second have stm32f103zc LQFP144 I can program LQFP100 model microcontroller using default SWD settings , but at the LQFP144 model i ...
Posted on February 06, 2013 at 02:21Hello guys,when I initialize for example this Interrupt:NVIC_InitStructure.NVIC_IRQChannel = OTG_FS_IRQn; I suppose it will have OTG_FS_IRQHandler as it's handler, but where can i look this up? I already searched...