STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI Sends Dummy bytes

Posted on March 05, 2013 at 14:32Hello All, I am using STM32F207VC. I have problem while sending data to slaves. I send a packet of data for example 0x01,0x02,0x03,0x04,0x05,0x06. While sending these packets SPI sends 0x00 in between anyof these da...

USART and wifi

Posted on January 30, 2013 at 12:34The original post was too long to process during our migration. Please click on the attachment to read the original post.

pietro2 by Associate II
  • 4576 Views
  • 6 replies
  • 0 kudos

STM32f407 and bootloader

Posted on March 05, 2013 at 11:52Hi Is it possible to change the pins of the bootloader that is loaded inside the chip? As I read it is only usart3 and  only on PORTB. Thank you

sami by Associate II
  • 893 Views
  • 1 replies
  • 0 kudos

full printf redirection

Posted on March 05, 2013 at 10:29Hello,I work with Atollic and STM3220 kit. I use the console with SWV. When I use printf with ''tiny_printf.c'' I have no problem.This is the method:in syscalls.c_write int (int file, char * ptr, int len){/ * Impleme...

pcu by Associate II
  • 821 Views
  • 2 replies
  • 0 kudos

Timer Synchronization

Posted on February 26, 2013 at 21:26Hello!Use stm32f107vc.I'm trying to synchronize two timers (TIM3 and TIM5), as including the external trigger. Configure them, as described in RM0008 page 386:void TIM3(void){RCC->APB1ENR |= RCC_APB1ENR_TIM3EN;TIM...

maryuriy by Associate II
  • 3360 Views
  • 9 replies
  • 0 kudos

Systick handler problems

Posted on March 01, 2013 at 04:44Dear,     I want to test the systick clock frequency. And use the systick as the RTOS system timer. It would be set to 1ms. And I use the configuration of the demo code as following:  if (SysTick_Config(SystemCoreClo...

xinjin by Associate II
  • 2566 Views
  • 7 replies
  • 0 kudos

Using the encoder mode with TIM4

Posted on March 04, 2013 at 21:06Hi all, I'm using an STM32F4Discovery (it's and STM32F407VGT6 on it).I'm trying to use the TIM4 timer to read a quadratic encoder (plugged on PB6-PB7), but somehow, it doesn't work.I'm using exactly the same code wit...

Background CRC32 in segments on STM32F4

Posted on March 01, 2013 at 22:32I would like to do a background CRC32 on FLASH such that I do 256 bytes at a time and get a final result.  The system must continue to run and meet RT deadlines while the CRC is calculated.  Additionally, communicati...

STM32L151 standby Power Consumption

Posted on March 04, 2013 at 15:21The original post was too long to process during our migration. Please click on the attachment to read the original post.

eva2 by Associate II
  • 1579 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.