Stm32F4 dma -> usart int is never called no output on usart
Posted on January 09, 2013 at 13:40The original post was too long to process during our migration. Please click on the attachment to read the original post.
Ask questions, find answers, and share insights on STM32 products and their technical features.
Posted on January 09, 2013 at 13:40The original post was too long to process during our migration. Please click on the attachment to read the original post.
Posted on March 06, 2013 at 13:06Hello everybody!I'm using timer TIM7 on STM32F407 to generate an interrupt on overflow. It works fine except one thing. When I enable the counter at first time it rises an interrupt immediately, right after setting t...
Posted on March 15, 2013 at 14:29Hi, I am trying to do 256pt-FFT on Audio data. The data is in stereo( LR) format. When I am doing FFT on only 1 channel data i.e Left then my system is running fine but as soon as I apply FFT on Right channel the sys...
Posted on March 14, 2013 at 20:07 I modify TIM Time Base example for learn more about timer, i blink led with timer, my code works well but i didn't understand instructions This is my code: /** ***************************************...
Posted on March 15, 2013 at 09:19Hello!I have a question about DfuSeCommand.I am pleasure to see your ungraded Dfuse.DfuSeCommand is added in the Dfuse.But I can not find out an introduction of DfuSeCommand.Do you tell me?Thank you.
Posted on March 12, 2013 at 10:07Hello, I have a problem when I try to connect IAR to the STM32F207 by the JTAG protocol. I have no problem when I use SWD instead of JTAG. I made a test with a J-Link probe and the SEGGER J-Flash ARM software, and I ...
Posted on February 23, 2013 at 13:50Hello ; I am getting Hard Fault exception when excutting the function arm_cfft_radix4_f32(&S,testInput ); I set the FPU on I tried to increase the heap and stack too but I could not solve it ; could you help ...
Posted on March 14, 2013 at 16:09 Hi, I got the a problem regarding the BOOT process, I don't know how to move the nBOOT1 pin. I have tried via software with the FLASH functions but with no good result. Also I am working with the J-link no with...
Posted on March 13, 2013 at 22:23Hi, I have a project with a STM32F205 and I was wondering if I can have two USB profile loaded. I want to have the ''mass storage'' profile as well as the ''HID''. Is it possible? My second question is regarding the ...
Posted on January 18, 2013 at 15:12 Hi all, I am using a DiscoreryF4 board to develop a small application that counts pulses entering a specific pin. This is required to read the pulses from a field instrument that generates the pulses as...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.