STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USART don't send what I want

Posted on April 04, 2013 at 22:20 First of all, sorry for my bad english and possibles gramatical mistakes; I'm working on stm32f100rb (Discovery Board). Well, when I want to sent a Ascii Character, for example, ''A'', I use the next comm...

manespgav by Associate II
  • 3611 Views
  • 8 replies
  • 0 kudos

STM32F2 LSE RTC crystal issue: Can anyone help?

Posted on March 01, 2013 at 13:45HelloWe use the STM32F2 for a project and have problems with the LSE crystal.We use a Citizen CMR200T crystal (32.768kHz, CL=6pF, Farnell Nr. 1652560) wich has a gain margin of 6.1 (according to the ST application no...

ter by Associate II
  • 1532 Views
  • 2 replies
  • 0 kudos

Interrupts are not occurring in order

Posted on April 03, 2013 at 16:55 Hi! All, I have a reed switch based Wind Speed and wind direction sensor(anemometer), these two reed switches(one for wind speed and another for direction) are connected to pull ups so that it generates the d...

The best way to compare two buffers

Posted on March 30, 2013 at 10:49Hello, I�m begineer in programming in C and microcontrollers, so I�m sorry for stupid question. I receive commands via USART. What is the best way to compare RxBuffer with command saved in memory? Now I use comparing...

j3lda by Associate II
  • 1735 Views
  • 2 replies
  • 0 kudos

SysTick_CALIB, What does it do??

Posted on April 05, 2013 at 01:35Using the STM32L152RB....So I know that the value stored in the SysTick_CALIB register is the value that must be loaded into SysTick_LOAD in order for the ticker interrupts to have a delay of 10ms (as stated in onlin...

F2/F4 I2S Ext.Clock

Posted on April 03, 2013 at 14:19Hi friends, It is written at ref/man for F2 and F4:Bit 7:0 I2SDIV: I2S Linear prescaler I2SDIV [7:0] = 0 or I2SDIV [7:0] = 1 are forbidden values. Why ''0'' is forbidden is clear, but why ''1'' ?! I make some intensi...

Using RTC to show time on LCD

Posted on April 04, 2013 at 11:52Hello,I'm new to embedded programming and having a hard time getting into using the STM32L-Discovery. I'm trying to use the RTC to display time on the LCD on the board, I've been reading the documentation but haven't...

Best TCP/IP Stack for STM32F2

Posted on April 03, 2013 at 21:46HI, I'm going to extend my project with TCP/IP stack. What do you think is a best choice for TCP/IP stack. Currently I'm hesitating between lwIP and uIP.  I'm developing under yagarto. Currently my code runs FreeRTO...

dimax by Senior
  • 2043 Views
  • 4 replies
  • 0 kudos

Timer problem

Posted on April 05, 2013 at 03:40Hi guysI want to do an experience with stm32f4.I want to simulate AM(amplitude modulation).I want to use 168 MHz as a carrier and generate the data in 100 khz. and modulate this 2 waves together.this action like i pu...

imanpakii by Associate III
  • 1007 Views
  • 1 replies
  • 0 kudos

JTAG Boundary Scan with ScanExpress

Posted on April 04, 2013 at 22:17My company uses a nifty tool called ScanExpress that takes your netlist, parts list, and BSDL files for the JTAG chain and creates an automated test using the Boundary scan to see if all the connections are correct. ...

wmoyne by Associate II
  • 922 Views
  • 0 replies
  • 0 kudos