STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Too Slow TFTP transfer speed

Posted on May 17, 2013 at 07:13Hi All I am using TFTP example in my project using STM32F2x7_ETH_LwIP_V1.1.0  library but my problem is about the transfer speed !! my results explain that a 255KB file transfer from Pc to ARM take about 3 minutes to c...

Program received signal SIGTRAP, Trace/breakpoint trap.

Posted on May 18, 2013 at 15:10Hello,I'm currently working on the STM32F100C8, but i'm having problems when trying to program it.When launching the debugger i get the following error:''Program received signal SIGTRAP, Trace/breakpoint trap.0x0800044...

PSRAM and LCD conflict ?

Posted on May 02, 2013 at 16:22Hi , I am getting a little problem with my LCD. It run well on my old board with fsmc. It was connected for FSMC_Bank1_NORSRAM1 fsmc_a16 was the RS pin and declaration was : #define LCD_REG              (*((volatile un...

warcatz by Associate II
  • 3645 Views
  • 11 replies
  • 0 kudos

STM32F407 BOOTLOAD options? URGENT!

Posted on May 17, 2013 at 08:47This is a continuation of my other thread on JTAG, but shifting topics slightly. I need to understand boot up and firmware loading/updating options better. I'm using the BGA version of this device in my product design....

STM32F3Discovery Compass Demo

Posted on April 28, 2013 at 14:11HelloI'm a student and my problem is, that I have to do compass demo on my PC, in order to do magnetic effect test. I bought STM32F3Discovery, but i can't find anything. I have found on youtube this compass demo, but...

kyniek by Associate II
  • 3108 Views
  • 9 replies
  • 0 kudos

Reading PSR

Posted on May 16, 2013 at 10:00HiDoes anybody have some inline GCC assembly to read the PSR? I am coming from an IAR background and in IAR I just used __get_PSR(), but this is not available in GCC - CrossStudio for Arm from Rowley. Any help in readi...

Gawie by Associate III
  • 1314 Views
  • 1 replies
  • 0 kudos

stm32f103 usart

Posted on May 16, 2013 at 07:49How can i use printf() with usart, if i want to dump the values on serial window after reading the register and printing it's value. #rtfm #stm32l #usart #usart #discovery

aman by Associate II
  • 2455 Views
  • 5 replies
  • 0 kudos

Running SPI at 2MHz

Posted on May 15, 2013 at 23:21I've got an STM32F407 with main clock set to 168MHz and am communicating with a slave device over SPI2. The SPI on the slave can work up to 2MHz and I would like to get as close to this as I can. As far as I can tell, ...

iduffy by Associate II
  • 2674 Views
  • 4 replies
  • 0 kudos

stm32f103 usart

Posted on May 16, 2013 at 07:52How can i use printf() with usart, if i want to dump the values on serial window after reading the register and printing it's value. #usart #discovery #stm32 #duplicate-thread

aman by Associate II
  • 1033 Views
  • 1 replies
  • 0 kudos

SPI Rx data reading error

Posted on May 15, 2013 at 13:32The original post was too long to process during our migration. Please click on the attachment to read the original post.

andykim by Associate II
  • 1600 Views
  • 2 replies
  • 0 kudos