STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UART baud rate error stm32f4xxG

Posted on July 25, 2013 at 14:46Hi All,I am using an evaluation board with 12MHz HSE. I used the the stm32 clock configuration tool to generate system_stm32f4xx.c file.My HSE frequency was 12 MHz, AHB clk was 24MHz and APB1, APB2 clocks were 12 MHz....

khalid by Associate II
  • 1109 Views
  • 1 replies
  • 0 kudos

Looking for a competitive STM32 reference

Posted on July 24, 2013 at 16:33Hi all,I had good experiences on STM32F4 peripherals, and I look now for a competitive price STM32 reference (I found STM32L152C6 is the cheapest, but I'd appreciate your feedback a lot) that could match that features...

neoirto by Associate II
  • 1133 Views
  • 2 replies
  • 0 kudos

problem with wakeup from stop mode

Posted on July 23, 2013 at 21:42Hi, I've got some difficulties with wake uC up from stop mode. Firstly I copied example from Std Periph Library for STM32F103: it uses alarm from RTC to wake up. I implemented it and everything was OK. But next - I tr...

kkkuba by Associate II
  • 2370 Views
  • 6 replies
  • 0 kudos

STM32 timer sets CC interrupt flags on overflow

Posted on January 06, 2012 at 23:59I found that when output compare registers are loaded with a value that is more than ARR, then on overflow the timer automatically sets compare match interrupt flags.  Has anyone seen it? #stm32-timer-inerrupt

ADC - Continuous mode stops after one conversion

Posted on July 19, 2013 at 13:16I am trying to use the ADC to convert continuously, but I am getting only one conversion each time I start the ADC ??? I am trying to use the ADC in 'analog watchdog' mode, monitoring a single regular channel (channel...

s_ by Associate III
  • 979 Views
  • 1 replies
  • 0 kudos

nonblocking sdio driver possible?

Posted on July 23, 2013 at 08:01Hi all,I'd like to implement a nonblocking version of the sdio driver. I'm using the stm2310e eval kit. The sdio driver provided uses a busy wait. Is it possible to modify this into a queue based nonblocking version? ...

st-link for stm32f3discovery

Posted on July 22, 2013 at 11:49Hello I am facing problem to download st-link/v2 for stm32f3 discovery for linux.plz guide me or give me some links realted to that.

SRAM with Hardware parity checking: What's that?

Posted on July 23, 2013 at 15:03In the summary for the STM32F050C4 device (and also for other STM32F0 devices, e. g. STM32F030), I find the statement: ''4 Kbytes of SRAM with HW parity checking'' This term also appears in the summary list at the be...

flyer31 by Senior
  • 2618 Views
  • 4 replies
  • 0 kudos

STM32F4: TIM Triggered SPI Transmit

Posted on May 13, 2013 at 23:27 Hi, I am trying to interface the STM32F4Discovery board with an external A/D-converter. The A/D generates a GPIO interrupt as soon as the data is sampled and ready to be retrieved. After that 3 * 8 bytes h...

tkurmann by Associate II
  • 3844 Views
  • 8 replies
  • 0 kudos

STM32F3 Discovery issue with ST Link v2

Posted on July 22, 2013 at 18:50Hello all,After toiling with the stlink v2 for awhile I've finally caved and decided to try my luck here.  The issue is that I've attached the st link SWDIO, SWDCLK, GND, and VDD on the evaluation board.  I installed ...

mahan2009 by Associate II
  • 2437 Views
  • 5 replies
  • 0 kudos