STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F407 RTC timestampping

Posted on July 25, 2013 at 11:06Hi All,I wanted to timestamp external events with a resolution of 10's of milliseconds. How can I do that in STM32F407 ?Best Regards,K #rtc

khalid by Associate II
  • 2320 Views
  • 4 replies
  • 0 kudos

stm32 and accumulator

Posted on July 29, 2013 at 14:24I have a question, I'm doing the robot. Is it possible to feed the controller from the battery and usb or is it dangerous?

svarog995 by Associate II
  • 1096 Views
  • 1 replies
  • 0 kudos

Virtual COM Port CDC on STM32F4-Discovery

Posted on July 29, 2013 at 11:59Hi all,I try to implement a CDC Device on STM32F4-discovery.I made an IAR project based on the VCP example project of the STM32_USB-Host-Device_Lib_V2.1.0.The STM32-Discovery starts correctly but two ''STM32 Virtual C...

pfifre by Associate II
  • 587 Views
  • 0 replies
  • 0 kudos

STM32F4Discovery counter problem,

Posted on July 28, 2013 at 22:22I have problem with timer - I want use one as simply counter of external impulses. Now I have (with too many unnecessary settings), but counter not work. I want use eg. TIM1, then I should use GPIO setting as AF for T...

alprof by Associate II
  • 1154 Views
  • 2 replies
  • 0 kudos

Strange PD2 behavior on STM32F405RG

Posted on July 25, 2013 at 10:40 Hi ! I'm trying to use PD2 on my STM32F405RG as GPIO output. I think i configured it correctly but it does not switch. Here is my code, it is not that difficult.... GPIO_InitTypeDef GPIO_InitSt...

Eich by Associate III
  • 2231 Views
  • 6 replies
  • 0 kudos

STM32F4 Discovery ADC+USART

Posted on July 28, 2013 at 19:03Hallo Guys,I'm working on project which implies analog to digital conversion and at same time transfering the converted data to the PC through the serial port. I've read couple of examples and was led to the following...

mahmoud by Associate
  • 1695 Views
  • 2 replies
  • 0 kudos

UART interrupts STM32

Posted on July 29, 2013 at 01:31I'm using UART for comunication with PC and I want to implement some interrupts. It seems to me that USART_IT_TXE  and  USART_IT_TC  are the same. Can someone explane me what is the difference between them? #stm32-...

marko by Associate II
  • 1206 Views
  • 1 replies
  • 0 kudos

Basic SDIO on F4 discovery board

Posted on September 15, 2012 at 09:58Can anyone please provide me with a link to some basic, low level, 4-bit SDIO interface code compatible with the STM32F4VGT? I'm not looking for it to support a file system(yet), I just want to be able to read by...