Posted on July 29, 2013 at 15:49help again, I work with a four-timer but it does not work the channels one, two and three. I initialize them but they do not give a PWM.CH4 working very good!My code:void init_pwm( void){ TIM_TimeBaseInitTypeDef TI...
Posted on July 29, 2013 at 14:24I have a question, I'm doing the robot. Is it possible to feed the controller from the battery and usb or is it dangerous?
Posted on July 26, 2013 at 22:19In the TIMER4 has four channels, I use all four channels to generate a PWM signal. How to stop a single channel, but that the other three channels continued to generate a signal?Thanx :D
Posted on July 26, 2013 at 22:06Hi! please help to solve the problem. I use a compass and a compile-time compiler gives me the following:Error[Li005]: no definition for ''SYSCFG_EXTILineConfig'' [referenced from C:\Users\Ëåâàí\ Error[Li005]: no defi...
Posted on July 27, 2013 at 08:45I check all the way for sure! All hooked up wrong! Completely copied the design of the examples and just did their friendly names for the compass function. I just checked everything, all the way true, where is the mis...