Posted on August 08, 2013 at 10:46Hi, i am using STM32F303 and I use ADC1 and ADC3, sometimes ADC3 doeset work Do I need to enable dual adc or is this recquired when ADC1 and ADC2 are used tnx
Posted on July 29, 2013 at 01:31I'm using UART for comunication with PC and I want to implement some interrupts. It seems to me that USART_IT_TXE and USART_IT_TC are the same. Can someone explane me what is the difference between them? #stm32-...
Posted on July 09, 2013 at 23:45The original post was too long to process during our migration. Please click on the attachment to read the original post.