STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Smt32w SampleMac 2 library - simplest project

Posted on August 14, 2013 at 10:59I try to make minimal progect from exaples, but they use EVAL librarys for demo board. Can i make minimal progect use SimpleMac library without HAL library and EVAL library? #smt32w-samplemac

ADC regular channels vs injected channels

Posted on August 12, 2013 at 13:52Hello,Can somebody kindly explain the difference/ different usage scenarios of ADC regular channels and injected channels?As per available documentation, it is mentioned injected channels are intended, when the conv...

SysTick_Handler suspended during other interrupts

Posted on August 13, 2013 at 17:12Hello Allm I am prototyping with the STM32 F3 Discovery board and using the ST standard peripheral library.  I am also using some example code that contains a function - Delay() - which uses the SysTick_Handler to d...

STM32F37x SRAM size

Posted on August 13, 2013 at 14:23Hi, I have a simple question regarding internal SRAM size of STM32F373Rx processor. Datasheet (rev.3, table 2 on page 10) specifies SRAM size of 24kB for 128kB Flash units,but I can read and write up to 32kB of SRAM...

bpacan by Associate II
  • 1672 Views
  • 2 replies
  • 0 kudos

Generating a fixed number of pulses on trigger

Posted on August 08, 2013 at 23:31Hi,I have what is essentially a timer question. I am interested in using an STM32 F4 (more RAM, higher clock speeds) for an application. My application requires me to generate a pulse every 2ms, pulse length ~100 us...

srsinha by Associate II
  • 2304 Views
  • 5 replies
  • 0 kudos

Help to create large buffers in RAM

Posted on August 12, 2013 at 21:48 Hello guys, I need some help. I want to create a large buffer in the sram and I'm having some problems with the compiler. I want to use the 112KB SRAM memory (pag 52 - RM0090) for my buffer. But when I w...

Sample a timer on EXTI interrupt

Posted on August 12, 2013 at 20:35Hi,I want to sample a fast timer (125ns) when an EXTI interrupt occurs, before the interrupt is handled. Later when the interrupt is handled i want to be able to compare the actual value of the same timer and measur...

STM32F3xx: I2S master clock

Posted on August 12, 2013 at 14:30Hi I tried to turn on the master clock for the SPI/I2S bus on the STM32F3 microcontroller by setting the MCLK enable variable in the initialization struct for the I2S 2. But I couldn't get any signal on the PA8 or o...

Flash Write Address

Posted on August 12, 2013 at 16:53I'm working on writing one byte to flash at the beginning of my program (the ID of the board).  I have been able to find a lot of examples of people rewriting their user flash and thus using the user address as the ...

mattfox by Associate II
  • 1473 Views
  • 2 replies
  • 0 kudos