STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

temperature sensor for stm32f4discovery

Posted on August 21, 2013 at 17:07Could anyone kindly through me a working example for the temperature sensor. I have build one on my own but have no way to verify it (use a glass of ice water?). So I'd like to see how someone else wrote the code. T...

ran2 by Associate III
  • 3161 Views
  • 7 replies
  • 0 kudos

timer15 update interrupt

Posted on August 22, 2013 at 16:11 hi, i'm using an f3 disco board and i want to configure its timer 15 with an update interrupt. i want it to be interrupted every one second to toggle two on-board LEDs. following is the code for timer15 and ...

hendalage by Associate II
  • 1891 Views
  • 3 replies
  • 0 kudos

STM32F103C8: Master full-duplex SPI problem

Posted on August 22, 2013 at 09:54Hi all, I am using a STM32F103C8 as a master in a SPI communication to an external ADS. My project has other interrupt sources, so I am not using additional interrupts for this SPI communication.The communication d...

juan by Associate II
  • 2527 Views
  • 7 replies
  • 0 kudos

STM32F051 IAP w/o a pushbutton

Posted on August 15, 2013 at 21:45Hi,We are developing a product using a STM32F051 and want to be able to upgrade the code using IAP. I've been reading anything I can find, AN4065, the examples, etc. It seems like the general idea is that the micro ...

munger by Associate II
  • 1247 Views
  • 4 replies
  • 0 kudos

ADC with STM32F303VC

Posted on August 19, 2013 at 07:48I want read ADC of STM32F303VC then display status  on three LED (If ADC>1000 LED red bright,ADC<500 LED green bright and extant LED ogrange bright) programmed code below,but i don't find error.Thanks everyone!#incl...

bee by Associate II
  • 2240 Views
  • 5 replies
  • 0 kudos

Missing doc on STM32l100 flash/eeprom programming?

Posted on August 20, 2013 at 12:11Hi everyone, I'm currently developing a product based on a stm32l100r8 mcu. I'm unable to find a document (akin to pm0062 for stml152) about flash/eeprom programming for this chip. Is this document available somewhe...

STM32L_Discovery Blinking LEDS

Posted on August 21, 2013 at 09:12I have an STM32L-Discovery Board, I found this program compiled it and loaded it on my board but nothing happens.  What am I miising..  Thanks in Advanced. CM.GPIO_InitTypeDef (GPIO_InitStructure); int main() { GPIO...

STM32F103 TIM3 Timebase problem?

Posted on August 21, 2013 at 16:41My timebase for TIM3 does seem to obey the laws of timebase calculation! I think I've had this problem before, what am I doing wrong.TIMCLK = 36MHz  TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;  /* TIM3 clock enab...

kkarasti by Associate II
  • 3054 Views
  • 5 replies
  • 0 kudos

Change IWDG reload and prescaler live

Posted on June 07, 2013 at 17:32Following my last post on the subject of flash memory erase vs watchdog I have another concern.Reading the spec I believe that I may be able to change the prescaler+reload of my watchdog just for the time that the fla...