STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F0 Discovery -> Demo source hard faults???

Posted on November 04, 2013 at 05:13I got the IAR tool chain installed and downloaded the discovery kit firmware package from the page:http://www.st.com/web/catalog/tools/FM116/SC959/SS1532/PF253215 I open the STM32F0-Discovery-Demo and then in IAR ...

STM32W and SimpleMAC Library

Posted on March 19, 2013 at 09:54The original post was too long to process during our migration. Please click on the attachment to read the original post.

STM32F429 and AMOLED screen

Posted on October 26, 2013 at 23:51Hello, for my project i need to connect HTC Desire screen to STM32F429. it has 800x480x16b resolution, RGB565 standart. To get best peformance, should i use original SDRAM (like in SDTM32F429i_DISCO board), or it ...

STRANGE HardFault_Handler in STM32F407

Posted on October 31, 2013 at 20:49Hi ; I have been trying to solve it with 4 days but I could not ! I have an old Project that I need to fix some bugs I have a bufffer defined as : float volt[1125]; in the new version I have to add pace_volt[18...

sami by Associate II
  • 2420 Views
  • 5 replies
  • 0 kudos

stm32f100 bootloader problem

Posted on October 30, 2013 at 21:11I tried to load the application code from my stm32f407 board to stm32f100 by rs232 and the bootloader inside the stm32f100.  I set the baudrate as 19200, 8bit, parity-even, one-stop bit per the application note. Ho...

mli by Associate II
  • 1382 Views
  • 2 replies
  • 0 kudos

Timer clock

Posted on October 31, 2013 at 15:17Hiwhen I set hclk to 72 for STM32F103 micro the timer doesnt work! I set APB1 pll to devide by 2, but in downt work aftar that alsowhats the problem? #too-vague

_behn4m by Associate II
  • 2911 Views
  • 8 replies
  • 0 kudos

Chaining 2 Timers - Pause the chaining effect

Posted on October 31, 2013 at 03:18STM32F4xxI have a setup where I am chaining 2 timers together with the internal trigger. TIMA is sending a TRGO to TIMB, which outputs in One Pulse Mode. This part works.What I want to do is to programatically tell...

dibs by Associate II
  • 1210 Views
  • 3 replies
  • 0 kudos

4-20mA to STM32 ADC

Posted on October 25, 2013 at 15:35How to input 4-20mA singnal to ADC in STM32? You know, ADC voltage is [0, 3.3V]. What circuit should add on the input? #4to20ma

ray by Associate II
  • 2885 Views
  • 1 replies
  • 0 kudos