STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using PH2 as GPIO

Posted on December 04, 2013 at 11:27 Hi, i'm using a STM32L151VD for a little project and i want to use the Port H2 as a normal Output for SPI CS. Using another Port (e.g. PC8) all works fine, but with PH2 it does not work at all. ...

jr777 by Associate
  • 1390 Views
  • 2 replies
  • 0 kudos

Split string -> default handler

Posted on December 04, 2013 at 00:05 hello everybody! I need help with my string splitter function. I use stm32f407 and CoIDE for develope. This is the function: char** str_split(char* a_str, const char* a_delim) { char** result =...

totti001 by Associate II
  • 2548 Views
  • 7 replies
  • 0 kudos

STM32F401 sampling now

Posted on May 14, 2013 at 19:37The http://www.st.com/pr-stm32f401 is the entry-level microcontroller in STMicroelectronics� high-performance http://www.st.com/pr-stm32f4 featuring the ARM� Cortex�-M4 32-bit/DSP core. While running at lower frequency...

USART Issues after wake up from stop mode

Posted on December 03, 2013 at 19:56Hello,I've succesfully started programming a STM32F0Discoveryboard: MCU is running on HSI (8MHz) at runmode.MCU is going into/outof stopmode every 5 seconds using the RTC running on LSE (32.768kHz)USART1 is conn...

r23 by Associate II
  • 3146 Views
  • 6 replies
  • 0 kudos

UART DMA STM32F4 Discovery

Posted on December 03, 2013 at 21:45 Hello I found an example of using DMA with UART on STM32F407 on this thread UART with DMA mode but i can't make it work. I use a STM32F4-Discovery and i try to see if DMA1_Stream2_IRQHandler is called...

9bit SPI Interface

Posted on December 03, 2013 at 09:26Hi. I want to know that there are any MCU which support 9 bit SPI interface. Do you know that? I will wait for your answer. Thanks.

andykim by Associate II
  • 1464 Views
  • 3 replies
  • 0 kudos

Problem with lwIP examples (STM3210C eval)

Posted on December 02, 2013 at 23:38I am recently working on lwIP. I have a STM3210C eval board.  I installed pragram codes. And I connected my board to modem using Cat5e ethernet cable. LCD is working, I think, that shows program is properly instal...

RTC TIMESTAMP when a TAMPER event occurs

Posted on December 03, 2013 at 22:32 Hello Guys, I am trying to make the RTC timestamp feature works but I couldn't. I have to detect a tamper event during anytime, even if the MCU is turned off, for this reason I have connected a batter...

SPI issue. CLK Signal with a Level

Posted on November 25, 2013 at 16:08 Hi everyone, I am trying to implement the SPI1 by hardware in my STM32F407VGT6, I did everything and actually it seems to work. But I was trying to read the ID from my SPI device (which is a Flash ...

0690X0000060MmCQAU.bmp

RTC - Timestamp when the RTC's power supply is VBAT.

Posted on December 03, 2013 at 17:51 Hi everyone, I am trying to figure out how make work the RTC timestamp feature when this peripheral is supplied by VBAT and when a Tamper detection occurs. And be sure about my RTC configuration...