STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 SPI-DMA error

Posted on December 06, 2013 at 14:18The original post was too long to process during our migration. Please click on the attachment to read the original post.

gcntrk by Associate II
  • 2703 Views
  • 4 replies
  • 0 kudos

custom IAP stm32f407

Posted on July 17, 2013 at 10:43Hi, I would like to add in-application programming (IAP) to my design. Of course, this is supported by the chip, with built in bootloader, etc. But in our system there are a number of chips distributed around the mach...

ian239955 by Associate II
  • 3864 Views
  • 9 replies
  • 0 kudos

Stm32l151rct6a Usart upto 4MBps! How?

Posted on December 10, 2013 at 10:16Hi,How can I increase the usart baud rate to 2MBps, 3MBps or 4MBps. Has anyone does this? Is there any sample code? #stm32 #stm32f4 #discovery #usart

periphe

Posted on December 10, 2013 at 12:32heloo,I have problem ? how to use the null-modem female/female RS232 cable between the DB9 connectr CN16 (USART3) and PC serial ??can you give me a picture please ?  #lmgtfy #first-principles #ask-better-questi...

tifou by Associate II
  • 1021 Views
  • 2 replies
  • 0 kudos

Unique device ID address in STM32F2xx

Posted on December 10, 2013 at 12:32Hi,I have been looking for some time and I cannot find an answer. In a previous project I found the UID for the STM32F107 using the following function. Can someone tell me what the equivalent for STM32F2 is?void G...

CAN communicatino problem discovery f4

Posted on December 09, 2013 at 20:45Hello I have a problem with CAN transmission and reception I have tried to make it connecting the CANRX to the CANTX, but it doesn't work. I have found the same problem when trying to make connection with other bo...

hadjrami by Associate II
  • 998 Views
  • 2 replies
  • 0 kudos

How to measure speed of STM32F429

Posted on December 10, 2013 at 06:34I have a STM32429I-EVAL board, initialized it and made it work, but I am not sure if the processor speed is up to max. The function RCC_GetClocksFreq returns 180 MHz, but cannot trust its return. I did a loop to t...

STM32F4 Discovery as SPI slave with interrupts

Posted on June 13, 2013 at 11:08hi,  I am working on  a project where I need to sample some data using the ADC in discovery at 1MSPs and transfer it to a raspberry pi board via SPI. As Rpi supports only SPI master mode the discovery board acts as a ...

Suggest an Eval Kit for STM32F101CB ?

Posted on December 09, 2013 at 06:37Hi, I am in search of Evaluation Kit for STM32F101CB , I am bit confused about picking a right evaluation board for this processor :( Can anyone please suggest me a good evaluation environment for STM32F101CB  ??...

STM32F0 CPAL I2C

Posted on June 01, 2013 at 17:23I'm trying to use to CPAL library to send data between I2C1 and I2C2 devices. I use STM32F0DISCOVERY. I2C1 is master, I2C2 is slave. In logic analizer I see that master send addres of slave but no ACK from slave. In ...