User Activity

Posted on April 22, 2012 at 20:52Hi, working with the STM32F103 processor, I`m searching for a solution to sychronize a STM32 timer to an external input signal. This signal has a constant frequency of e.g. 24Hz or 30Hz. Using a input capture timer...
Posted on April 17, 2012 at 15:01Hi, I want to capture a signal with 30Hz frequency by a timer input capture. The timer is already working but the measured frequency is not 30Hz. I always measure a frequency of 29.85Hz or 30.3Hz. Are there any mist...
Posted on April 11, 2012 at 20:46Hi, I`m working with the STM32F103XC processor (lqfp144 package) and I want to use the input capture mode for the Timer1. At the moment I didn`t get any timer interrupt while the I/O PE13 has a lot of rising edges. ...
Posted on October 22, 2010 at 16:03STM32F103VC JTAG Chaining possible?
Posted on October 21, 2010 at 22:16STM32F103V performance high enough?