STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Setting up HSE on STM32F4 Discovery

Posted on December 12, 2013 at 15:48 I'm sure there's probably already a post on how to do this, but I can't find it so here goes: I'm trying to set up the external 8 MHz oscillator on the F4 Discovery. I'm using Keil IDE and have set my...

USART communication via RXNE interrupt only reads one char

Posted on December 11, 2013 at 22:37Hello ST Community,I am using a STM32F2 uC for my project, and I have configured an USART interface as an UART by not initializing the clock settings. In order to program the device the UART is connected to I send...

dmg0048 by Associate II
  • 2467 Views
  • 3 replies
  • 0 kudos

Certificate Management for Embedded Devices

Posted on December 11, 2013 at 20:24One of the building blocks that we see most commonly misunderstood is how to manage SSL certificates in embedded devices. For this reason we have designed a whitepaper that provides an introduction to SSL certific...

wilfred by Associate
  • 1200 Views
  • 0 replies
  • 0 kudos

Problems with the configuration of the Input Capture Filter

Posted on December 11, 2013 at 14:33Hi community, i've got a question dependig on the configuration of the input capture filter of the stm32f407. I found the following lines in the datasheet (depending TIMx_CCMR1 register): =========================...

kurchr01 by Associate
  • 1735 Views
  • 2 replies
  • 0 kudos

STM32f427 clock system

Posted on December 11, 2013 at 11:43Hi,Is there the possibility to achieve the maximum CPU clock speed (180MHz) with the USB clock at 48MHz??According my calculations, to have USB clock of 48MHz I need to reduce the CPU clock to 168MHz, instead of 1...

ababo by Associate II
  • 2420 Views
  • 4 replies
  • 0 kudos

[STM32F2xx] Running code from ram.

Posted on August 02, 2011 at 11:00Hello,I'm using tasking which allows easily to tag methods to be copied in ram at startup and then run them from ram.But I'm wondering at which extend it is a good idea ...On the one hand, run from ram means zero wa...

root by Associate II
  • 1215 Views
  • 3 replies
  • 0 kudos

EWARM breakpoints not working....

Posted on December 11, 2013 at 11:57The subject line is not strictly right. I can set breakpoints but not on all of my code. Here is the story so far.I have written some code for the STM32F0 Discovery board. The code runs both SPI ports as masters, ...

jason23 by Associate II
  • 1440 Views
  • 3 replies
  • 0 kudos

STM32L Discovery I2C issue

Posted on December 10, 2013 at 08:57  The original post was too long to process during our migration. Please click on the attachment to read the original post.

klemen by Associate II
  • 1300 Views
  • 1 replies
  • 0 kudos

LSM303DLHC Data Ready

Posted on December 10, 2013 at 10:37Anyone can help me in configuring the LSM303DLHC data ready interrupt 1 on the  32F401CDISCOVERY board. I enabled it by writing on CTRL_REG3_A but i can see it only when i read manually a full set of data

andiob by Associate II
  • 1021 Views
  • 1 replies
  • 0 kudos