STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Solved: STM32F4Discovery EXTI Multiple Interrupts

Posted on January 03, 2014 at 03:17 EDIT: Solved by clive1! See post below. Hi (again), I'm tinkering with Interrupts this week. I'n the example code I have provided below, The Green light flashes (as expected) in the loop....

Just Matt by Associate III
  • 1268 Views
  • 2 replies
  • 0 kudos

MAX485 and STM32 ?

Posted on January 01, 2014 at 01:49Guys, Can I use MAX485 and STM32F107VCT6? I can't find VH max on F107 datasheet, is it possible if I interface MAX485 with STM32F107VCT6 USART ? pin PA9 and PA10 connected directly to MAX485 Any clues ? Thanks #...

STM32 PWM output blocked ?

Posted on January 27, 2011 at 15:17STM32 PWM output blocked ? #pwm-systick-dma-nvic #tim4 #pwm #pwm #stm32f #tim4 #stm32f103 #outputs

hanser by Associate II
  • 5629 Views
  • 13 replies
  • 0 kudos

UART to CAN in STM32F103RB ???

Posted on January 01, 2014 at 15:11 Hello Friends, Using STM32F103RB how can it be done: --->>RS232(RX Recieve Message)---(Process Message)--CANBUS(Transmit Meesage)---> Wait for response(interrupt, poll vs.)...--->CANBUS(Recieve Meesage) --(Proces...

aybala5 by Associate II
  • 2601 Views
  • 5 replies
  • 0 kudos

high STOP mode current

Posted on August 22, 2012 at 17:29In STANDBY mode my board current drops to 300uA which is as expected. However if I use STOP mode it is 880uA. I had expected STOP mode to be only 20 - 30 uA more than STANBY. In STOP mode I turn all pins to analog i...

trevor23 by Associate III
  • 2819 Views
  • 6 replies
  • 0 kudos

Cannot Connect to STM32F405RGT6 on Breakout (ST-Link V2)

Posted on December 25, 2012 at 14:43Hello all,I created my own breakout board for the STM32F405RGT6, but I'm unable to connect to it via the ST Link V2. The error is ''No Target Connected''.I've tested this with an external 8Mhz crystal (with load c...

honboxuan by Associate II
  • 12623 Views
  • 39 replies
  • 0 kudos

Hard fault Exception when bus fault exception occured

Posted on December 31, 2012 at 19:28Dears, I have problem while debuging the code for STM32L151RDT6. I get every time the hard fault exception with bus fault. Description of Project: I am using KEIL 4.54 with ST Link/V2. The system has SPI FLash (8M...

Bipolar ADC possibility

Posted on December 31, 2012 at 16:49I will use the STM32 to drive a power supply.  The input signals to the ADC do not need any gain, so I'd like to avoid using as many OPAmps as possible.  The problem is that many of the potentials are negative or ...

drobison by Associate II
  • 3566 Views
  • 5 replies
  • 0 kudos

Temporarily suspending SPI

Posted on December 29, 2012 at 01:28I've got a mixed-signal board with an LCD connected through noisy SPI lines. When the display is being updated, the analog readings are all over the place. In addition to improving the layout of the board, I'm als...

andyturk by Associate II
  • 2187 Views
  • 3 replies
  • 0 kudos