STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UART received value conversion to float

Posted on December 30, 2012 at 21:28I have been working on a program to directly transmit any character or set of characters that I transmit from the PC via UART, back to the PC immediately. This is just the first step in my project. Code (this work...

Segger J-LINK vs ST-LINK/V2?

Posted on December 29, 2013 at 21:25I'm currently using a ST-LINK/V2 to develop code for STM32F205/7, but am wondering if I would be better off with a Segger J-LINK. What's the difference in capabilities between these two? I using the Atollic IDE/co...

amoore by Associate II
  • 3286 Views
  • 1 replies
  • 0 kudos

Transfer variable contents from STM32F4 to MATLAB

Posted on December 28, 2013 at 14:27I would like to know if there exists a sample code on which I can elaborate to do the following:Transfer data stored in a variable on the microcontroller to computer software such as MATLAB through the USB OTG int...

TIMx External trigger

Posted on December 28, 2013 at 15:22what is the difference betwee TIM2_CH1_ETR and TIM2_ETR? I'v only found TIM2 has the TIM2_CH1_ETR, all other TIMs, such as TIM1, TIM3, TIM8, only have TIMx_ETR. I'v also found the problem that only TIM2 can be tri...

STM32 and VS1003

Posted on September 12, 2013 at 17:12Guys, Does anyone of you have experience on interfacing VS1003 with STM32? Any ideas or links will be appreciated, Thanks #interface-anything-to-anything

Overruns with Back-to-back USART Rx DMA on STM32F05x

Posted on December 17, 2013 at 00:05We're using a UART to pass control information between two STM32 parts.  The bit rate is 500Kbaud which gives us about 20us per byte.  The aim is to use DMA to receive the byte stream in the background and process...

eleventen by Associate III
  • 676 Views
  • 1 replies
  • 0 kudos

Does STM32L100RC have opamps?

Posted on December 27, 2013 at 03:00Hi, I'm posting for the first time here. Does STM32L100RC have opamps? I'm asking this because I am finding conflicting information: When I go to: http://www.st.com/web/en/catalog/mmc/FM141/SC1169/SS1295 and click...

ETH_Start() sometimes failed to start mac

Posted on December 17, 2013 at 10:26Hi My product is based on stm32f407, the Ethernet works well normally, except that, sometimes(10% possibility) after the MCU powered up or hot rebooted, the mac can transmit packets, but can NOT receive.  When thi...

shark by Senior
  • 2288 Views
  • 5 replies
  • 0 kudos

STM32F4Discovery (FSMC) + FT2232H

Posted on September 12, 2013 at 04:07 Hello, I have paired up an STM32F4Discovery board with an FT2232H part from FTDI. The purpose of this is to use the CPU-FIFO mode of the FTDI part for faster USB data transfer. I made the necessary mo...

mehmoodn by Associate
  • 1980 Views
  • 1 replies
  • 0 kudos