cancel
Showing results for 
Search instead for 
Did you mean: 

keil problem Error #136

sami
Associate II
Posted on April 18, 2013 at 18:41

Hello

I have a struct in my code ;

typedef struct

{

unsigned char  volume;

unsigned char  l_bat;

unsigned char  h_bat;

unsigned char  rtc;

unsigned char  pace;

unsigned char  child;

 unsigned char date;

unsigned char  day; 

unsigned char  month; 

unsigned char  year;

unsigned char  hour;

unsigned char  min; 

unsigned char  motion;  

signed char    gmt;

unsigned int delay[10];

unsigned int shock[3];

char language[3];

}settings;

but the comp?ler give an error for one member

..\src\main.c(452): error:  &sharp136: struct ''<unnamed>'' has no field ''date''..

I can use the other members but not date!!!

what is wrong here ... ?

Thank you

#unproven-fix
This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
Posted on April 18, 2013 at 19:26

what is wrong here ... ?

Something else. You probably have something else defined as date, perhaps another typedef.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
sami
Associate II
Posted on April 18, 2013 at 20:56

Infact no .. there is no otherdate ,  even though when i change  the member date to other words..still give the same error.. that is really crazy...

Thank you

sami
Associate II
Posted on April 18, 2013 at 22:22

Upgrading to 4.70 solved the problem ..strange
Andrew Neil
Super User
Posted on April 19, 2013 at 08:15

Trouble is, if you don't know what was causing the problem originally, and you don't know why it's now gone away - how can you be sure that it's really fixed?

You may still have a latent bug which just happens not to manifest - yet...

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
sami
Associate II
Posted on April 19, 2013 at 11:37

It is was strange error .. that I have never seen it .

The compiler can accept all stuck member but not date .. even if i change date to any other word .. it seems it was related to stuck size .. not sure .. after upgrading it is ok .. Even keil guys could not make better reply more than suggest to upgrade ..

However , now after upgrading non of my 3ulink2 work! even after upgrading them ! strange ..

Thanks

frankmeyer9
Associate II
Posted on April 19, 2013 at 11:49

Have you tried to make your struct non-anonymous ?

Just in case the compiler has some problems with that.