STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Release mode have problem

Posted on January 22, 2014 at 07:50Hi all,I am using IAR v6.6, but I can not config project on release mode, when I select release mode, I still can dubug the code, but it must remove debug code on mode release.Maybe I wrong config, please help meTh...

np1 by Associate II
  • 2022 Views
  • 6 replies
  • 0 kudos

spi1 work well only in debug mode

Posted on January 22, 2014 at 09:41i am trying to communicate between stm32100rb discovery value and transceiver cc2500 via spi1. for checking, i wrote a value to the cc2500 to specific register, and then, i read the value of this register, and prin...

STM32F4 DMA large block transfer

Posted on January 21, 2014 at 09:41Hello to all,I am writing application which uses peripheral to memory DMA transfer. When transfers aresmaller than 65535 items written in NDTR register everything is working fine.To be able to support large piece o...

Change IWDG timeout at runtime

Posted on January 22, 2014 at 15:20HiI'm porting a software from STM32F101/STM32F103 to STM32F0x family of uC. I need to change the watchdog timeout during runtime. On the F101/F103 this worked. On F0x it seems to fail. For me it looks as if after a...

hug by Associate
  • 1279 Views
  • 0 replies
  • 0 kudos

L6218E Error

Posted on January 21, 2014 at 19:54The original post was too long to process during our migration. Please click on the attachment to read the original post.

kqian by Associate II
  • 1536 Views
  • 3 replies
  • 0 kudos

warning marker for vcp program

Posted on January 17, 2014 at 23:28Hey Guys, After I programed vcp for STM32F427 Eval board by following the example of STM32F429Discover board, but when I plug it into the PC, The PC can find it but always get a warning marker on the Device manager...

0690X00000602qrQAA.jpg
kqian by Associate II
  • 1899 Views
  • 10 replies
  • 0 kudos

Assembly Code Example

Posted on May 01, 2013 at 00:02I've made up a board and embedded a STM32F4 on it.  I want example assembly code to compile and upload to the chip.  I can't find any on the entire internet for a Cortex-M4.  Does anyone have a link to a generic GPIO b...

drobison by Associate II
  • 9799 Views
  • 25 replies
  • 0 kudos

STM32F401CC Clock configuration

Posted on January 21, 2014 at 18:00Hello,We are developping an application on STM32F401CC mcu and we are not sure that our clock configuration is correct because, when we are setting baud rate of USART1 or USART2 greater than 115200 bps, data exchan...

vincent by Associate II
  • 1536 Views
  • 1 replies
  • 0 kudos

STM32F0 SWD Lockout

Posted on January 20, 2014 at 19:43 Hi Everybody, i'm trying to get some of the STM32F0 peripherals (in this case GPIO, SysTick, NVIC, SPI, DMA) working. Im using IAR EW 6.7 + IAR I-Jet (which is connected via SWD to the Chip). A...

twalter by Associate II
  • 1509 Views
  • 3 replies
  • 0 kudos