STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32l100 data structure alignment,packing and pading

Posted on March 26, 2014 at 09:09Hello, I'm using stm32l100(compile and debug through kiel v4) which is connected to Network processor (Lon ft5000) ,.my firmware consist of structures and nested structures with different size of members ,...My doubt...

sundar by Associate II
  • 1136 Views
  • 1 replies
  • 0 kudos

STM32F103R8T6 Timer4 Input Capture problem

Posted on March 24, 2014 at 11:17Hi!There is a problem with Timer4 Input Capture use.  Initially everything was developed under the STM32L100R8T6 controler, but so happened that it was necessary to pass to STM32F103R8T6. This code perfectly works at...

gambit by Associate II
  • 4697 Views
  • 13 replies
  • 0 kudos

Manchester Decode with EXTI interrupt and Timer count

Posted on March 26, 2014 at 00:32 Hello, I want to decode manchester code sent by RFID chip EM4 I set up a timer as counter without interrupt and EXTI line with interrupt. I am getting an interrupt on every rising and falling edge of the PC.6...

Flash is corrupting after a couple of immediate resets

Posted on March 23, 2014 at 20:11 I want to store Device ID inside the flash permanently. So I am using internal Flash of STM I can write&read to Flash in STM After writing the value to the flash, and switch off and then I can read it without any...

io517 by Associate
  • 2776 Views
  • 5 replies
  • 0 kudos

wrong device marking STM32F100RCT6

Posted on March 23, 2014 at 07:57I have chosen STM32F100RCT6 for a new project because of the large number of PWM channels it has. I was not able to activate the clock for timers 12-17, therefore I conduct some more experiments with this chip. Surpr...

Strange MCU behaviour by passing pointer to stucture

Posted on March 24, 2014 at 13:44 Hi All, I'm running some code on Discovery STM32L152 board. I'm getting Hard Fault each time I initiate structure fields in a function: 1. void pid_Init(float p_factor, float i_factor...

Tom by Associate II
  • 2133 Views
  • 8 replies
  • 0 kudos

stm32f0 interrupt

Posted on March 24, 2014 at 18:59Hi,i want to start an interrupt to leave the sleep mode after a precise that my ADC reads.Could some body help me and put what i shall do in a nut shell?thank you for your attention PS: i am using an stm32f0 discover...

d4ng3r09 by Associate II
  • 1226 Views
  • 4 replies
  • 0 kudos