STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F42xx errata - FMC Corruption ... really?

Posted on March 27, 2014 at 11:19The STM32F42xx and STM32F43xx Errata DocID023833 Rev 6 Para 2.8.4 says, there may be Corruption of data read from the FMC under some circumstances. ''When the FMC is used as stack, heap or variable data, an interrupt...

John F. by Senior
  • 1197 Views
  • 2 replies
  • 0 kudos

USB HID or CDC

Posted on March 12, 2014 at 11:01Hi, I have implemented the CDC(VCP) class on my F3 discovery and it work very well. Now, i want to send a integer data each 25µs. So i have to set up my rate speed of my board to 1600Kbps.On the PC side, the speed ra...

hilwan by Associate II
  • 7578 Views
  • 15 replies
  • 0 kudos

stm32x405, can't program through stlink v2

Posted on March 16, 2014 at 22:54Dear all, after some issues using a programmer as parport interface, i am trying to program stm32f405 with a cheap stlink-V2, but still without success. I attach the openocd log, maybe someone can help me. Open O...

Angelo1 by Associate II
  • 1507 Views
  • 2 replies
  • 0 kudos

STM32F439xxx as graphic controller for DVI output

Posted on March 26, 2014 at 21:00Hello, for application in medical devices we need to develop a DVI interface to drive a commercial LCD monitor. We are analizing the usefulness of the STM32F439xxx serie as graphic controller. We only will display im...

alimed by Associate II
  • 2639 Views
  • 6 replies
  • 0 kudos

stm32f0: effect of bootloader on usart

Posted on June 25, 2013 at 10:58Hi there, I'm using ST's bootloader in rom to program my device and USART1 for communications. Now I observed the following problem: when my code runs directly after startup, it works fine. However, when my code recei...

a2 by Associate II
  • 2103 Views
  • 4 replies
  • 0 kudos

ADC Question

Posted on March 27, 2014 at 03:52 Hi , I am reading up on STM32F4 ADC and have problem understanding a few points . ADC_InitStructure.ADC_ExternalTrigConv =ADC_ExternalTrigConv_T3_CC1 ; ADC_InitStructure.ADC_ExternalTrigConv =...

what is speed of GPIO?

Posted on March 27, 2014 at 02:25I'm really wondering what speed selection of GPIO is.There are some options to select GPIO Speed, such as 2MHz, 25MHz, 50MHz and 100MHz.What does the speed mean?Which value is selected generally?

twoaten by Associate II
  • 2555 Views
  • 4 replies
  • 0 kudos

USART STM32F4 PROBLEM

Posted on March 26, 2014 at 20:51Hi, I have an error in my code and I can not seem identifying the problemThe erreur is : ..\main.c(97): error:  #169: expected a declarationThis is my code /***********************************************************...

haythem by Associate II
  • 2092 Views
  • 8 replies
  • 0 kudos