Skip to main content
ckern
Associate II
May 14, 2013
Question

STM32 HS USB DMA Transfer

  • May 14, 2013
  • 3 replies
  • 2271 views
Posted on May 14, 2013 at 23:02

Is it possible to use DMA for USB transfers? My understanding of the STM32 DMA controller is that it will transfer data from one place to another without CPU usage. If I were moving data from RAM to a DAC output, I can easily see (and have coded) this. But for transfer out to a USB peripheral, I would think that the CPU would be needed to operate the USB interface. Is this correct? 

I am trying to read from one high-speed interface (~8MBd) and transfer the data via USB. I would like to use the DMA USB transfer at the same time as I am using the CPU to read in the next set of data. Is this possible? Thanks. 

-- Chris 

#stm32f207
This topic has been closed for replies.

3 replies

mikroforma
Associate
June 14, 2013
Posted on June 14, 2013 at 17:05

yes, I have exactly same question. Can STM32 USB  do bulk HS transfers directly from external memory without loading CPU?  (that would involve DMA obviously).

Has anybody tried anything similar?

Tesla DeLorean
Guru
June 14, 2013
Posted on June 14, 2013 at 18:11

It strikes me that the USB FIFO buffers are accessible by the DMA controller. DMA2 in M2M?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
tsuneo
Associate II
June 15, 2013
Posted on June 15, 2013 at 19:31

STM32F2/F4 OTG_HS core has an embedded DMA controller, which connects to SRAM1,SRAM2 and FSMC over the multi-layer AHB. As the default, STM32_USB-Host-Device_Lib_V2.1.0 enables this DMA for OTG_HS. In this version, the DMA transfer occurs in the unit of packet (transaction). Though the data tranfser is done by DMA, ARM core intervention is still required to start/finish each transaction, to set up OTG_HS registers (the stack code takes care of this process at all).

> I would like to use the DMA USB transfer at the same time as I am using the CPU to read in the next set of data. Is this possible?

You may apply double buffer or a cyclic buffer.

While the ARM core preares the next packet, pass another (portion of) buffer to DCD_EP_Tx().

DCD_EP_Tx() accepts any size of transfer, even greater than MPS (Max Packet Size) of the bulk endpoint.

https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex_mx_stm32%2Fstm32f207%20usb%20%20only%20multiple%20of%2064%20bytes%20can%20be%20send

> Can STM32 USB  do bulk HS transfers directly from external memory without loading CPU?

Set up FSMC for an external SRAM.

Pass a buffer on the FSMC address space to DCD_EP_Tx() or DCD_EP_PrepareRx()

Tsuneo