STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F401 -- SPI Slave Receiving 32bit word

Posted on April 30, 2014 at 23:57I have a SPI master device that transmits data in 32 bits while NSS is active. Since the STM32F401 SPI can only be configured as a 16bit SPI port, I am wondering if I can still make it work. Will the SPI port continu...

dibs by Associate II
  • 545 Views
  • 0 replies
  • 0 kudos

Facial recogniction and eigenface

Posted on April 30, 2014 at 14:38Guys, Does anyone of you have experience on using eigenface for comparing the image from camera ? Any references ? thanks #cross-post

STM32LXX eeprom initialized data

Posted on April 26, 2014 at 10:33Hi I use STM32L151CC it has embeded EEPROM data 8KB, I now how to write or read from this memory, but I don't now how to initialize data in eeprom when I programming device. Someone knows how to do it? I use GCC comp...

wilkxt by Associate II
  • 847 Views
  • 2 replies
  • 0 kudos

STM32Cube generated project, adding to HAL driver

Posted on April 29, 2014 at 22:22I'm having trouble during the Link stage after adding a component to the HAL driver in my project. I'm using IAR. I generated a project using STM32CubeMX. I then manually added use of the RTC component, by including ...

kartik by Associate II
  • 2295 Views
  • 4 replies
  • 0 kudos

Bootload on STM32f107RCT (64PIN)

Posted on April 29, 2014 at 19:16In AN2606:''Workaround�? For 64-pin packagesNone. The bootloader cannot be used.�? For 100-pin packagesDepending on the used peripheral, the pins for the unused peripherals have to be keptat a high level during the b...

ecos port on STM32

Posted on April 30, 2014 at 13:47Hi every body,Is there somebody who has ecos port on stm32 in standalone and can share it.Thanks in advance.

Timing issues with sram and lcd on fsmc bank 1

Posted on April 29, 2014 at 15:13Hello I really hope someone has been down this road before :) I have a hard time getting my sram and lcd working together on fsmc bank 1. I use a STM3221G-EVAL for testing, with it's 16Mbit SRAM and a ILI9341 LCD. Bo...

bk by Associate II
  • 1484 Views
  • 2 replies
  • 0 kudos

Problem in creating waveforms with the help of timer

Posted on April 29, 2014 at 11:44 Hi All The waveform.png file I have attached to show what i have to do. I have to generate similar kind of waveform with using one timer . The timer clock is 168 MHz...... One waveform will be 2 clock on and...

sanjib by Associate III
  • 1760 Views
  • 7 replies
  • 1 kudos

Driving_motor_using_pwm

Posted on April 25, 2014 at 08:44The original post was too long to process during our migration. Please click on the attachment to read the original post.

sanjib by Associate III
  • 2659 Views
  • 7 replies
  • 0 kudos

Read PWM input without TIM

Posted on April 30, 2014 at 04:29Excuse me, I want to ask, can I know duty cycle of PWM without using TIM? I thought if I can read the time of PIN either in high or low logic and then divided by period. So I can measure the duty cycle. Assumption : ...

liviana by Associate II
  • 937 Views
  • 1 replies
  • 0 kudos