STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM3221G-EVAL ETHERNET

Posted on May 31, 2014 at 16:51I'm a student of University of Tunisia and I'm using IAR Embedded Workbench for ARM, v. 7.10, 32K Kickstart Edition on WIndows 7...I am currently alternating, and my first project is to establish communication between ...

STM32F030K6 device issue

Posted on June 02, 2014 at 11:22In this device(STM32F030K6), CLK & DIO signals for SWD are in portA (PA13&PA14). But unknowingly I have changed the default settings of portA(PA13-dio, PA14-clk) and flashed the program. so I want to erase the flash m...

abilashs by Associate II
  • 5184 Views
  • 14 replies
  • 0 kudos

Spi 3 problem STM32F429

Posted on June 03, 2014 at 11:30HelloIn our project we need the Spi 3 channel to control an Oled display. The display is connected to pins: D6, B3 and B4 so the Spi 3 pins need to be remapped to those pins.The remapping is done in the spi3 init func...

m_ by Associate II
  • 1147 Views
  • 2 replies
  • 0 kudos

I2C EEPROM M24C64 sequential read

Posted on June 03, 2014 at 12:55 Hello, I'm looking for source code example of i2c eeprom library for STM32F2xx which is not using DMA. Especially I'm looking for sequential read function. Please if you know any links, post it. I...

bogusz by Associate II
  • 1059 Views
  • 0 replies
  • 0 kudos

i found the adc of stm32f103ret6 is nonlinearity

Posted on May 29, 2014 at 16:56hi, i am using stm32f103ret6 to test the voltage from the signal genarator(DG1022 from rigol). i found the adc of stm32 is nonlinearity. i found that,when the voltage from DG1022 is less than 1V,the voltage get from ad...

Manage memory in STM32F407

Posted on June 02, 2014 at 06:49Hello everyone today I have one problem with my manage memory I run freeRTOS in stm32f4 board (Cortex M4), I create one task. This task execute regular expression program (source code for regexp from: http://www.argli...

STM32 Cube Java JRE Issue

Posted on February 21, 2014 at 06:22I tried to run the new STM32Cube MX and I am getting a program needs JRE1.7.45 or newer.  I just installed the latest JRE, now just labeled 7 update X and it still will not launch.  I then tried to uninstall the p...

STM32F407 ADC DMA TIM interrupts

Posted on May 31, 2014 at 17:55  The original post was too long to process during our migration. Please click on the attachment to read the original post.