cancel
Showing results for 
Search instead for 
Did you mean: 

Testing USART1 on STM32F429I-DISCO board

H UQ
Associate II
Posted on October 28, 2013 at 15:22

Hi All,

I am working on USART1 device for STM32F429I_DISCO board. [I have already tested my serial device (code) on stm32429i_eval1 board.]

I am using following USART setup/pin mapping

unsigned int temp;

/* Enable GPIOA on AHB1 */

ENABLE_PERIPHERAL_CLOCK(AHB1, GPIOA);

/* Select Alternate Function 7 for USART1 pins */

temp = GPIO_READ(A, AFRH);

temp &= (0xFFFFF0FF & 0xFFFFFF0F);

GPIO_WRITE(A, AFRH, (temp | (0x00000700 | 0x00000070)));

/* Select Alternate function for USART1 pins */

temp = GPIO_READ(A, MODER);

temp &= (0xFFCFFFFF & 0xFFF3FFFF);  

GPIO_WRITE(A, MODER, (temp | (0x00200000|  0x00080000)));   

/* Enable Clock for USART1 */

ENABLE_PERIPHERAL_CLOCK(APB2, USART1);

My Questions are

Can we test USART1 on STM32F429I_DISCO board?

If yes, then above mentioned pin mapping is correct?

If yes, then should we use JP4[TX, RX]  pins for this purpose?

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Posted on October 28, 2013 at 15:35

You could attach a USB-to-CMOS Serial type adapter and confirm it that way.

You could connect PA9/PA10 with a wire or micro-jumpers, and prove it looped back.

You could use a MAX3232 or equivalent type device to generate RS232 levels and add a DB9.

For JP4 to work you'd need to do something with SB11/SB15, but that would connect you too the STM32F103 part, which may/may-not provide the serial connectivity you want. I'd suspect NOT.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
H UQ
Associate II
Posted on October 30, 2013 at 16:15

Thanks for reply

For this option

>>>> You could connect PA9/PA10 with a wire or micro-jumpers, and prove it looped back.

Is USART support Loop back mode? It is not mentioned in reference manual

For this option

>> You could use a MAX3232 or equivalent type device to generate RS232 levels and add a DB9.

I have tried to use this option but i receive garbage characters (funny characters) on tera term all the time.

My USART driver works fine without any change [RCC, CLOCK; mentioned above] on STM32429I_EVAL1 board but not on DISCO board.

Should I do some thing more regarding GPIO/RCC/CLOCK settings?

Have any one tested USART1 (PA9/PA10) on this board (STM32F429I_DISCO)

Moreover in one of the thread [[DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Discovery/Help%20me%20USART%20STM32F4&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F&currentviews=210]Help me USART STM32F4], you have mentioned that

>>> You haven't explicitly stated that you're using an STM32F4-Discovery board, but if you are PA9 is not usable for a USART pin due to a huge bulk capacitor being attached to it.

It means PA9 can not be used for USART testing?

Posted on October 30, 2013 at 17:00

I'm talking about a piece of wire externally (looping back), this will not be discussed in the manual. You send a character, you should receive a character. Functionality of pin confirmed, baud rate implicitly the same.

You have a different board, right? So comments about an

http://www.st.com/web/en/catalog/tools/FM116/SC959/SS1532/PF252419

aren't going to impact a completely different design. Check the schematics.

Baud rates look wrong, or junk on terminal. You can measure bit times on a scope. Most likely you have wrong HSE_VALUE and/or PLL settings. The

http://www.st.com/web/catalog/tools/FM116/SC959/SS1532/PF259094?icmp=stm32f4pr_pron_p3436s_sep2013

has an 25 MHz HSE, the

http://www.st.com/web/catalog/tools/FM116/SC959/SS1532/PF259090

has an 8 MHz HSE. Settings for one won't work with the other, timings, and expectations will be different. Computation for USART baud rates are predicated on knowing what the clocks actually are.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
H UQ
Associate II
Posted on November 08, 2013 at 15:04

Thanks for fruitful response.

Successfully tested the serial driver by

  • using '' USB-to-CMOS Serial type adapter'' with PA9 and PA10 pins
  • Updating HSE_VALUE (8MHZ) and PLL settings