cancel
Showing results for 
Search instead for 
Did you mean: 

Is SDIO >4 GB issue fixed in the latest library?

dmg0048
Associate II
Posted on November 10, 2013 at 15:59

Hello ST Community,

I plan to connect a uSD card with my STM32F207 using the SDIO 4 bit bus interface and Chan's FATFS. Searching on the forums I've encountered a few problems with the code provided in the Standard Peripherals Library regarding the incompability with >4 GB cards, however these problems were reported on 2011 and the latest code dates from March 2012 as shown here:

  * @file    stm322xg_eval_sdio_sd.c

  * @author  MCD Application Team

  * @version V5.0.3

  * @date    09-March-2012

  * @brief   This file provides a set of functions needed to manage the SDIO SD

  *          Card memory mounted on STM322xG-EVAL evaluation board.

At the moment I can't test this with hardware so I've been lurking the code for a while and I haven't found anything that suggests me this bug has been fixed. Before attempting to fix it myself I would like to ask if I missed something and the bug is really fixed, because it seems a bit odd to me that this issue hasn't been resolved when it has been reported a year prior to it's release, and I've also checked the release notes and I haven't found anything other than the generic 'Bug Fixes' statement.

Thanks in advance!

#sdio-4gb-4bits-issue-bug-fatfs
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on November 10, 2013 at 16:13

ST's solution is to extend byte addressing variables to 64-bit. Block devices are accessed at a block level, and thus there are needless conversions back and forth.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
dmg0048
Associate II
Posted on November 11, 2013 at 11:47

True, I re-checked the libraries again and I just noticed on the release notes .html the utilities directory this issue was fixed the way you mentioned, I guess I've missed it but all in all my issue is resolved.

I will see if this solution is viable with my project and in case it isn't I will attempt to fix it by myself, I've read on some other thread you patched some Discovery libraries to make it work with >4 GB cards so I already got a good start point ;).