STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

European Workshops - Manchester June 17th

Posted on June 13, 2014 at 14:17Hi,Just wondering if anyone else has signed up for this workshop? I signed up with about 4 others but we're not sure if it's still happening or not? These events need at least 8 attendees to go ahead and we can't get ...

jono-tree by Associate II
  • 2439 Views
  • 5 replies
  • 0 kudos

Dropped GDB connection after STM32F373 Clock Configuration

Posted on June 13, 2014 at 19:33Hello all,I'm currently working with a custom board fitted with an STM32F373. I'm programming it using an STM32F3 Discovery board through the st-link-v2 interface. Previously, I was able to successfully connect with O...

Resolved! STM32 nucleo-L053 - systick code

Posted on June 11, 2014 at 22:54Hi, I used CubeMX 4.2 to generate code skeleton for L053. I have no problem with simple programs (LED blinking, etc). But I cannot use systick. I understand that HAL_init() takes care of setuping the systick. Unfortun...

UART STM32F429 & STM32F407 discovery

Posted on June 13, 2014 at 09:05Hi, I'm testing the two discovery STM32F429 and STM32F407. What I've done so far is that the 429 sends data to the 407 through UART4. The 407 interrupts at every character received, and all works fine! If I do the opp...

ccm use in keil

Posted on June 13, 2014 at 08:35Dear all ,i want to use the ccm (stm32f407) at the keil uVision , but i did't find the way how to write the scatter file ? could you give me a way how to use the ccm in the keil ? thank you . #ccm

FPU in IAR IDE

Posted on June 12, 2014 at 18:22Hello,        I am using the STm32F4 discovery demo board and using the IAR IDE tool chain, Can anyone tell me how to use(enable) the Floating Point unit.Thanks for ur help.RegardsSameer  

Simple Timer TIM7 ''update event''

Posted on June 12, 2014 at 02:03 Why do I get an immediate update event when I configure TIM7 like this: TIM7->CR1 = 0; TIM7->PSC = 7199; TIM7->ARR = 2000; TIM7->DIER = 0; TIM7->CNT = 0; TIM7->CR1 = TIM_CR1_CEN; while ((TIM7->SR & TIM_SR_UIF...

gene by Associate II
  • 2232 Views
  • 5 replies
  • 0 kudos

STM32L051 Development

Posted on May 25, 2014 at 19:09Folks, The STM32L051 looks like a good device for a new project, but there seems to be no-one stocking it and there seems to be no dev kit. Can I use the STM32F0 discovery and any code will be essentially drop-in when ...

DiBosco by Senior II
  • 1308 Views
  • 3 replies
  • 0 kudos

STM32F100C6, ADC & DMA

Posted on June 09, 2014 at 21:37 Hello, I have a problem with configuring ADC & DMA. This is the code ADC RCC -> APB2ENR |= RCC_APB2ENR_ADC1EN; ADC1 -> CR1 |= ADC_CR1_SCAN; ADC1 -> CR2 |= ADC_CR2_EXTSEL_0 | ADC_CR2_EXTSEL_1 | ADC_C...

peter_l by Associate II
  • 1979 Views
  • 4 replies
  • 0 kudos