STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VCP driver for linux embedded

Posted on June 16, 2014 at 16:22Hi, I have STM32L1 work with STM32 VCP library The VCP work very well in windows, but I need work in the linux embedded with kernel 3.11I tried but linux does not detect the STM32 VCP, while the FTDI work very well in...

problem when compiling fft_excample with gcc

Posted on June 18, 2014 at 12:54Hello, i'v try to compile example fft code using stm dsp libraries. Got this error message: /usr/gcc-arm-none-eabi-4_7-2013q1/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib/armv7e-m/fpu/libm.a(lib_...

teijo by Associate II
  • 848 Views
  • 1 replies
  • 0 kudos

Problem with I2Cx_EV_IRQHandler called way too frequent

Posted on June 18, 2014 at 11:17Hi, I am new to this forum and to using the STM32 processors, so please forgive me if this topic has already been discussed. I am using a Discovery board with a STM32L152RC micro-processor on. I am trying to implement...

kennethf by Associate II
  • 1298 Views
  • 1 replies
  • 0 kudos

CAN driver

Posted on June 18, 2014 at 11:57So if I want to connect two discovery boards, Could I use this sample? I have to use 2 CAN driver?!!

0690X00000605YvQAI.png
hamed by Associate II
  • 628 Views
  • 0 replies
  • 0 kudos

SPI interruption problem

Posted on April 04, 2014 at 16:43Hi all,I would like to know if anyone has a problem when enabling the Tx buffer empty interrupt. In fact, when i put SPI_I2S_ITConfig(SPI1, SPI_I2S_IT_TXE, ENABLE);  , the code coming after can't be executed switch (...

ULPI HS-USB and I2S

Posted on June 17, 2014 at 05:07Without delving into the DS, can someone please confirm for me whether you can or cannot have ULPI and I2S enabled at the same time with F2-F4 QFP144 and smaller?This seems a bit odd since I think there would be a nee...

STM32F205 Power Stop example does not work

Posted on June 17, 2014 at 17:47Hello, I am currently trying to get the example code for Stop mode for the STM32F2xx processor to work, without success. The example in question is the Stop.ewp project. The Wakeup IRQ handler is never called and the ...

gerald2 by Associate
  • 1151 Views
  • 2 replies
  • 0 kudos

Looking for alternative STM32 peripheral libraries

Posted on June 12, 2014 at 16:11Hi, I'm in a project were we would like to use the STM32F103TBU7. As a toolchain we would like to use the IAR Embedded Workbench. Sadly I'm not allowed to use the STM peripheral library. This because it's a security a...