STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX wrong pin label

Posted on June 25, 2014 at 15:47Hi,Using STM32F405RGTx, pin 64 is labelled PDR_ON while datasheet contains VDD.Which one is the correct one ?Thanks.

STM32F334: the new STM32 Digital-Power Microcontroller

Posted on June 25, 2014 at 17:29ST’s new microcontroller http://www.st.com/web/en/catalog/mmc/SC1169/SS1576/LN1820 simplifies transition to energy-efficient digital power supplies by providing all the major power-control functions in a single chip. ...

STM32F401 reference manual

Posted on June 25, 2014 at 15:07I'm sure that this is a really silly question, but is there actually a reference manual for the STM32F401 chips? I can't see one on the design resources page. The STM32F401 Discovery documentation refers to ''RM0344''...

evan2 by Associate II
  • 1559 Views
  • 2 replies
  • 0 kudos

Sequence of ADC conversion in Regular Simultaneous Mode

Posted on June 18, 2014 at 14:34Hi Everyone In my project, I need to capture 6 channel ADC signals in Regular Simultaneous Mode. for that, I just started for 2 channels (Channel 0 in ADC1 & Channel 1 in ADC2). Since it does simultaneous conversion, ...

ss2 by Associate II
  • 3466 Views
  • 8 replies
  • 0 kudos

PDR_ON connection question

Posted on May 28, 2014 at 07:31We are using the controller STM32F427ZIT6 from ST in our design. As we are using the NRST pin for processor reset in our older design(Atmel AT91FR40162S-CJ) we are trying to Bypass the Internal Reset circuitry of ST.In...

Jumping to program from custom bootloader

Posted on June 22, 2012 at 20:42I have nearly got a custom bootloader working which downloads code using RS485 and is encrypted using xtea. I have done the following: 1. Recompiled the original program with the start address as 0x8003000 defined in ...

DiBosco by Senior II
  • 2895 Views
  • 7 replies
  • 0 kudos

Tutorial 1 for STM32CUBEF4 did not work

Posted on June 19, 2014 at 23:06Hi,I am following the instruction on UM1718 user manual, the section on Tutorial 1 from pinout to project C code generation using an STM32F4MCU). The following listed the codes generated by the code generator. I have ...

s23 by Associate
  • 1245 Views
  • 1 replies
  • 0 kudos

STM32CubeMX 4.3.0 FW1.2 Known Issues

Posted on June 24, 2014 at 00:54With the new version of MX I will try to consolidate all issue here:USB CDC bug in the new STM32Cube FW_F4 V1.2.0 library[DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=/public/STe2ecommun...

joe by Associate III
  • 1464 Views
  • 2 replies
  • 0 kudos