STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

IAR Embedded Workbench Support

Posted on June 26, 2014 at 16:07 Hi all, I have a project that I've been working with that I recently tried to send over to another person but they're encountering an error when trying to flash their part. The code compiles fine but the f...

daniel2 by Associate II
  • 1734 Views
  • 2 replies
  • 0 kudos

How is receiving of a i2c byte initiated?

Posted on June 27, 2014 at 04:05Hi, I would like te receive 3 Bytes. Therefore I am sending a start, the I2C address of the slave, the register address, a repeated start, the slaveaddress again, then I receive the 3 bytes and finish wish a stop. So ...

Loading software to ST board

Posted on June 27, 2014 at 00:54Hello Everyone,Our goal is to compile an AudioSpeaker Demo included in the STM32_USB-FS-Device_Lib_V3.3.0. The IDE being used for this project is the IAR Embedded Workbench for ARM version 7.20.1.7307, IAR Embedded Wo...

STM32F303xC CAN configuration.

Posted on June 20, 2014 at 17:12Hello everyone, i am trying to implement CAN on my application. It is the first time i am dealing with it. I've read a lot about protocol itself, and looked through a lot of examples which are posted in this forum. Th...

STM32F303 ADC/DMA

Posted on June 26, 2014 at 19:25I am using all 4 ADC's with 4 channels used on each. ADC 1 is on DMA1 and ADCs 2-4 have channels on DMA2.  All 4 ADC's run off timer15 at 1Khz.  The problem I am having is that I only get DMA interrupts for ADC 3,4 a ...

msinger by Associate
  • 1788 Views
  • 5 replies
  • 0 kudos

USB CDC bug in the new STM32Cube FW_F4 V1.2.0 library

Posted on June 22, 2014 at 12:16There is a bug on the latest STM32F4 usb cdc code. Update the STM32CubeMX and the STM32CubeF4 library to the latest versions. Create a new project and enable RCC HSE with external crystal and HS usb in device mode (in...

sdim by Associate III
  • 2058 Views
  • 4 replies
  • 0 kudos

STM32F105 problem jumping to application

Posted on June 23, 2014 at 15:35I have problem with jump to application by bootloader. The device used is the STM32F105R8. The bootloader does not jump in the application,it crashes in the function ''Jump_To_Application()''. The code of the bootload...

u23 by Senior
  • 3790 Views
  • 14 replies
  • 0 kudos

Update Usart baud rate register during communication

Posted on June 26, 2014 at 17:01Hello,I would like to know what happens if I modify the USART baud rate register value very little (+-3%) during a communication. Is it safe or is it essential to stop the communication before updating the BRR value e...

nicolas23 by Associate II
  • 1300 Views
  • 5 replies
  • 0 kudos

DMA2D configuration error

Posted on June 25, 2014 at 02:28 I'm trying to do a simple memory to memory transfer with the DMA2D, but the configuration error flag is being set when I start a transfer. Here is the initialization code: uint16_t *imageBuf = (uint16_t*)0...