User Activity

Posted on December 17, 2014 at 20:11Hi friends, Is it possible to handle 1553 bus with stm32 series microcontrollers without using asic or fpga (ip core). For CANbus there are can trancievers that can be directly connected to mcu in the circuit, but...
Posted on November 16, 2014 at 19:34Hello Friends, I have a stm32f4 discv. board and need to drive 6 motor drivers independently that have RS422 interface (just send command, no pwm calc.) How can i do that with discv board or in new designing ? Is ...
Posted on October 06, 2014 at 17:36Hello, I send a char string to com port using sym32f4( with 3 pins only: GND VCC TX) and listen using ''hercules'' program finded on the net. I get weird characters, took a screanshot and uploaded as attachment. Ca...
Posted on October 01, 2014 at 23:00Hello Friends,    I have an stm32f4 discv. board. I tried the run one of the STM32F4xx_DSP_StdPeriph_Lib_V1.4.0 examples without any change. I used template, copied one of the examples project files ( ...\STM32F4xx...
Posted on May 31, 2014 at 21:37Hello Friends, I bought stm32f4 discv. board and also http://www.aliexpress.com/item/1-pcs-MPU-6050-Module-3-Axis-Gyroscope-Accelerometer-Module-for-Arduino-MPU-6050-Worldwide-FreeShipping/1361575363.html board but i h...