STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Measuring power consumption of STM32F4DISCO's MCU

Posted on July 21, 2014 at 10:12Hello,I want to measure the STM32F4DISCOVERY's STM32F407VGT6 power consumption, is there someone who already done this ? I mean, is there a solution to plug an ampermeter in this kit's Vdd pin ?I saw that in another S...

STM32F4Discovery Exapansion kit - Ethernet connector

Posted on July 21, 2014 at 10:24Hello,When I connect an ethernet cable to the expansion kit, the RJ45 LEDs are not lighting, it that normal ? they are lit once, but after never even disconnecting the board. that's strange !With a PIC32 starter kit w...

SMBUS Clock Stretching Not Obeyed

Posted on July 02, 2012 at 00:05I am using an STM32F103 chip using I2C1 configured as an SMBUS Host (also tried normal I2C) to talk to a smart battery charger and smart battery.  The charger comms are fine both in software and look perfect on the lo...

0690X000006050jQAA.png 0690X000006050tQAA.png
pshields by Associate II
  • 3389 Views
  • 5 replies
  • 0 kudos

stm32f205rg spi configuration

Posted on July 21, 2014 at 11:47 hi,all I'm working on a SPI interface on stm32f205rg. I'm newly using this chip. I do the configuration as I do on stm32f103 and of cause refer to example of stm32f2. It's just not working. I configure SPI1...

838445810 by Associate II
  • 1111 Views
  • 2 replies
  • 0 kudos

offline IDE setup for nucleo-stm32F401

Posted on May 17, 2014 at 12:12Hi all, i tryed the online mbed compiler but it does not satisfied me and so i'm looking for an offline solution. Can you help me to setup an offline IDE like eclipse, netbeans or visual studio? Is this board like ardu...

allejp by Associate
  • 1191 Views
  • 2 replies
  • 0 kudos

USART2 TC interrupt timing

Posted on July 21, 2014 at 21:47I am using the TC (transmission complete) interrupt on USART2 to detect end of transmission of a packet.  I have noticed that the interrupt isn't triggered until approximately 3.5us after the last byte is transmitted....

Where are the VDDA/GNDA pins in the STM32F205RG?

Posted on July 21, 2014 at 16:07Hello, I'm using the STM32F205RG chip (WLCSP64 package) This chip has no dedicated pins for VDDA/GNDA. Are these connections shared with a specific VDD/GND pin? If so which one? The goal of my question is to make a n...

caruel by Associate
  • 916 Views
  • 1 replies
  • 0 kudos

STM32CubeMX - Where did GPIO 16-bit port access functions go?

Posted on July 17, 2014 at 16:31HiMigrating from STM32F4-Discovery_FW_V1.1.0 to STM32Cube_FW_F4_V1.3.0 firmware creates some difficulties with regards to GPIO port access.  The functions below are not available anymore or did I miss something?  Port...

frank2 by Associate
  • 1583 Views
  • 3 replies
  • 0 kudos

STM32CubeMX

Posted on July 19, 2014 at 22:33hi ,i am currently evaluating STM32CubeMX for STM32F4 , great tool for getting started on New MCU.I have few question : 1.How can i define User Code block ? so when i make changes to existing project    the STM32CubeM...

eyals111 by Associate II
  • 1238 Views
  • 2 replies
  • 0 kudos