STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC: first injected channel creates voltage peak

Posted on July 22, 2014 at 10:53Hello!I have a problem with the ADC on my STMF4Discovery Board.I am reading two analog voltages with ADC1 in triggered injection mode.The voltage on the pin with injection rank 1 always has a peak at the injection eve...

0690X000006058nQAA.png 0690X000006058sQAA.png

detecting edge in falling/rising mode interrupt

Posted on July 23, 2014 at 11:10I want to config external interrupt line 0 in both falling/rising edge mode. But I don't know how I can detect that event happen due to falling edge or rising edge. It should do different function for falling and risi...

STM32L151: Timer Capture Input (TIMx_CHy vs TIMx_ICy)

Posted on June 23, 2014 at 17:02Hi, I'm using a STM32L151 and would like to connect the pin PA2 to one of the timer capture inputs. According to the reference manual and the example InputCaptureRouting in the STM32L1xx_StdPeriph_Lib_V1.1.1, this cod...

Problem with DCMI FRAME interrupt ?

Posted on July 22, 2014 at 19:02Hullo guys , I 'm trying to get my OV7670 cam working with STM32F207zg , and I have set up all required configurations , I want to get snapshot , transfer the frame to external SRAM , but the FRAME interrupt is never ...

STM32L100 RI for TIM IC routing

Posted on July 10, 2014 at 04:57 Hi all, question on the STM32L100 RI. I'm trying to use the RI to remap PA12 to TIM4CH1. As soon as the GPIO pin is set to alternate function mode on AF14 it's immediately set to output low, regardless of RI->ICR...

Huge assert bug in STM32CubeMX V4.3 with STM32Cube V1.0

Posted on July 20, 2014 at 14:45There is a huge bug in STM32CubeMX with STM32Cub V1.0 when full assert is enabled.When I make a project with timers or SPI and full asser is enabled, then the program hit the assert when the HAL_init function is calle...

Osto by Senior
  • 1535 Views
  • 2 replies
  • 0 kudos

Error Flash download failed - ''Cortex M4''

Posted on July 18, 2014 at 12:14Hello, I´m doing my bachelor thesis at the moment by designing a hardware with a microcontroller. I´m using a self made board with the STM32F407ZG microcontroller. My board has a JTAG adapter for programming. All the ...

STM32F3 internal temp sensor

Posted on March 07, 2014 at 13:37The original post was too long to process during our migration. Please click on the attachment to read the original post.

arganasss by Associate II
  • 2990 Views
  • 9 replies
  • 0 kudos

Touchscreen TFT GLCD Display interfacing without FSMC?

Posted on July 22, 2014 at 13:56Hello All,I wonder if it is possible for me to interface a GLCD about 3-4'' size with a MCU which doesn't have FSMC in it? Is it possible? The price constraints i have for our product doesn't allow me to have a MCU wi...

venkat by Associate
  • 965 Views
  • 1 replies
  • 0 kudos