STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F0- Serial communication problem (USART 1)

Posted on July 29, 2014 at 08:36 Hi, I am trying to sent some data to the controller (STM32F051) via pl2303 connector. Data is sent from an application. The problem is, I'm not able to receive the data sent by the application properly. The d...

aruns06 by Associate II
  • 1493 Views
  • 2 replies
  • 0 kudos

How to make USB Audio Speaker work in STM32F303C-EVAL?

Posted on July 30, 2014 at 04:31Hi,Firstly, I tried to browse on the forums but there were only a few concerning STM32 F3-series.I have an STM32303C-EVAL board with STM32F303VCT6 MCU.I wanted it to act as a USB Audio Speaker.Basically:[PC] --USB--> ...

maggie by Associate III
  • 860 Views
  • 0 replies
  • 0 kudos

Unable to Set RTC on STM32F4

Posted on July 28, 2014 at 21:38Hi, I'm following an example as provided by the STD PERIPHERALS library, on an STM32F4 Discovery board. In spite of what's being written in the config routine, when I set the define for LSI, I read back this: Year = ...

DMA UART

Posted on July 29, 2014 at 20:26I am trying to send an array over UART using the DMA. I dont know why the DMA does not send more than 65535 elements.Is there a restriction on the DMA for only 16Bit numbers only ? #stm32f4 #board #discovery #rtfm ...

Change heap size in IAR embedded workbench

Posted on July 29, 2014 at 21:07HiI'm trying to get the USB virual com ports working with a STM32F401 discovery board, using IAR workbench, and the code generated from STM32 Cube MX. I found this/public/STe2ecommunities/mcu/Lists/STM32Java/flat.aspx...

bgeri91 by Associate
  • 2265 Views
  • 2 replies
  • 0 kudos

Reading Problem from ADC

Posted on July 29, 2014 at 00:53Hello,        I am reading from an external ADC in parallel interface(16 bits). I dont know what is wrong, only my port PE0 and PE1 are talking to the controller at 1V and rest all others taking at 3V. when I remove t...

DFU mode driver v3.0.4

Posted on February 03, 2014 at 17:30The DFUse software package (STSW-STM32080, version 3.0.3) comes with the USB Tube driver (STTub30.sys) version 3.0.1.  This driver works for me on Windows 7, but does not work on Windows 8 for me.  At some point i...

32L0538DISCOVERY

Posted on July 28, 2014 at 11:51Hi everyone,I apologize beforehand if this isn't the right place to post my question, but I just started with this forum :).Anyway, I've been given an STM32L0538-Discovery board for a project and I can't seem to find ...

zehpaulo by Associate
  • 1182 Views
  • 3 replies
  • 0 kudos