cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 USART receive problem

stefanskos9
Associate II
Posted on October 25, 2012 at 07:33

Hi,

I'm having problems receiving USART data on the F4. I can see the data is being sent from my LCD on my Saleae logic analyser, but the STM32 won't call the USART RXNE interrupt. I can send data no problems, just not receive Can anyone see a problem in my code?

void USART_Configuration(void){
// sort out clocks
RCC_AHB1PeriphClockCmd( RCC_AHB1Periph_GPIOD, ENABLE);
RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART3, ENABLE);
NVIC_InitTypeDef NVIC_InitStructure; // this is used to configure the NVIC
NVIC_InitStructure.NVIC_IRQChannel = USART3_IRQn; // we want to configure the USART3 interrupts
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;// this sets the priority group of the USART3 interrupts
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1; // this sets the subpriority inside the group
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; // the USART3 interrupts are globally enabled
NVIC_Init(&NVIC_InitStructure); 
// Configure LED USART3 Tx (PD8) as alternative function input floating
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOD, &GPIO_InitStructure);
// Map USART3 to D.08 
GPIO_PinAFConfig(GPIOD, GPIO_PinSource8, GPIO_AF_USART3); 
// Configure USART3 Rx (PD9) as input floating
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOD, &GPIO_InitStructure);
// Map USART3 to D.09 
GPIO_PinAFConfig(GPIOD, GPIO_PinSource9, GPIO_AF_USART3);
// Initialize USART
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Tx | USART_Mode_Rx;
// Configure USART3
USART_Init(USART3, &USART_InitStructure);
// Enable the USART
USART_Cmd(USART3, ENABLE); 
USART_ITConfig(USART3, USART_IT_RXNE, ENABLE); // enable the USART1 receive not empty interrupt 
}
void USART3_IRQHandler(void){
(do something)
}

Thanks for your help in advance!
This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
lowpowermcu
Associate II
Posted on October 25, 2012 at 09:59

Hi Stive,

In USART Rx configuration, try to change 

''

GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;''

by

''

GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;

''

Posted on October 25, 2012 at 11:59

You can try to use a polling based receiver, instead of interrupt, to ensure there is no problem with reception as such.

JW

Posted on October 25, 2012 at 17:35

Doesn't look hideous, although the IRQ routine needs to clear the interrupt.

I'm using USART3 PB10/11 with interrupts, seem to work fine for me.

Here is a quick IRQ demo for the STM32F4 Discovery board using PD8/9

// STM32 USART IRQ TX/RX Loop (USART3 Tx PD.8, Rx PD.9) STM32F4 Discovery - sourcer32@gmail.com

#include ''stm32f4_discovery.h''

volatile char StringLoop[] = ''The quick brown fox jumps over the lazy dog\r\n'';

/**************************************************************************************/

void RCC_Configuration(void)

{

/* --------------------------- System Clocks Configuration -----------------*/

/* USART3 clock enable */

RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART3, ENABLE);

/* GPIOD clock enable */

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);

}

/**************************************************************************************/

void GPIO_Configuration(void)

{

GPIO_InitTypeDef GPIO_InitStructure;

/*-------------------------- GPIO Configuration ----------------------------*/

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8 | GPIO_Pin_9;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_Init(GPIOD, &GPIO_InitStructure);

/* Connect USART pins to AF */

GPIO_PinAFConfig(GPIOD, GPIO_PinSource8, GPIO_AF_USART3);

GPIO_PinAFConfig(GPIOD, GPIO_PinSource9, GPIO_AF_USART3);

}

/**************************************************************************************/

void USART3_Configuration(void)

{

USART_InitTypeDef USART_InitStructure;

/* USARTx configuration ------------------------------------------------------*/

/* USARTx configured as follow:

- BaudRate = 9600 baud

- Word Length = 8 Bits

- One Stop Bit

- No parity

- Hardware flow control disabled (RTS and CTS signals)

- Receive and transmit enabled

*/

USART_InitStructure.USART_BaudRate = 9600;

USART_InitStructure.USART_WordLength = USART_WordLength_8b;

USART_InitStructure.USART_StopBits = USART_StopBits_1;

USART_InitStructure.USART_Parity = USART_Parity_No;

USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;

USART_Init(USART3, &USART_InitStructure);

USART_Cmd(USART3, ENABLE);

 

USART_ITConfig(USART3, USART_IT_TXE, ENABLE);

 

USART_ITConfig(USART3, USART_IT_RXNE, ENABLE); }

/**************************************************************************************/

void NVIC_Configuration(void)

{

NVIC_InitTypeDef NVIC_InitStructure;

/* Configure the NVIC Preemption Priority Bits */

NVIC_PriorityGroupConfig(NVIC_PriorityGroup_0);

/* Enable the USART3 Interrupt */

NVIC_InitStructure.NVIC_IRQChannel = USART3_IRQn;

NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;

NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

NVIC_Init(&NVIC_InitStructure);

}

/**************************************************************************************/

void USART3_IRQHandler(void)

{

static int tx_index = 0;

static int rx_index = 0;

if (USART_GetITStatus(USART3, USART_IT_TXE) != RESET) // Transmit the string in a loop

{

USART_SendData(USART3, StringLoop[tx_index++]);

if (tx_index >= (sizeof(StringLoop) - 1))

tx_index = 0;

}

if (USART_GetITStatus(USART3, USART_IT_RXNE) != RESET) // Received characters modify string

{

StringLoop[rx_index++] = USART_ReceiveData(USART3);

if (rx_index >= (sizeof(StringLoop) - 1))

rx_index = 0;

}

}

/**************************************************************************************/

int main(void)

{

RCC_Configuration();

GPIO_Configuration();

NVIC_Configuration();

USART3_Configuration();

while(1); // Don't want to exit

}

/**************************************************************************************/

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
thirukannan
Associate II
Posted on April 01, 2014 at 15:40

Hi,

I want to use UART1 with interrupt in STM32L151R8  . I tried based on your example but I am not getting the output .please help me through following mail id (thirukannan.perumal@eldaas.com)

I am waiting for your help .And advance thanks for your help.

Regards,

Thirukkannan P

(thirukannan.perumal@eldaas.com)

Posted on April 01, 2014 at 16:35

Yeah, that's not how forums work.

[DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Java/stm32l100%20UART&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000F9A0E3A95BA69146A17C2E80209ADC21&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Java/AllItems.aspx&currentviews=13]https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fSTM32Java%2fstm32l100%20UART&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000F9A0E3A95BA69146A17C2E80209ADC21&TopicsView=https%3A%2F%2Fmy.st.com%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2FSTM32Java%2FAllItems.aspx¤tviews=13
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..