STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F051R8 TMER3 ISSUE

Posted on September 22, 2014 at 16:48Hi.. In STM32F051R8 board, Iam using TIM3. I need to set timer interrupt for every every 10 seconds. Iam unable calculate the prescaler, CCR and time period values. Can any one explain me please...

stm32f4 discovery board is not working

Posted on October 09, 2014 at 08:47Hi everyoneI was working with stm32f4discovery board.It was working fine and i was able to execute my programs without any difficulties.Now after some day I am working with the same board.But my stm board is not ev...

How can I exit from standby mode using wakeup pin ?

Posted on October 08, 2014 at 17:48 Hi, I'm using an stm32f401 mcu, mounted above Discovery platform, trying to understand how can I correctly use the standby low power mode; for this reason, I use the PA0 wake up to exit from this low power...

DUrbano by Associate III
  • 3243 Views
  • 8 replies
  • 0 kudos

FFT on STM32F4

Posted on October 08, 2014 at 03:24Hi,Iam trying to use DSP lib on STM32F4 chip. I run the example project of FFT on CMSIS lib and it's ok:an float array ==> FFT ==> result   it's ok.But I try on my board:Signal generator => external ADC => FFT on S...

nhandt3 by Associate II
  • 2220 Views
  • 3 replies
  • 0 kudos

STM32F2xx SPI slave receive data problem

Posted on September 12, 2014 at 04:32I have a STM32F2xx connected to FTDI UM232H using SPI communication, STM will configured as Slave and FTDI as Master, I will be using NVIDI have configured my SPI as below: 2 line duplex1 Mhz clockMSB8bitPhase ...

ho by Associate II
  • 976 Views
  • 1 replies
  • 0 kudos

SPI TX trouble on F4

Posted on August 14, 2014 at 19:39 I have an SPI setup using DMA transfers that works for a while, and then reaches a point where the data that is passed to the DMA transfer is not what is sent over the SPI lines. Typically, I am able to success...

jwoolston by Associate II
  • 1805 Views
  • 3 replies
  • 0 kudos

Problem using RS485 on STM32F030R8T6

Posted on October 02, 2014 at 17:27 Hello, I am trying to initiate a RS485 communication with the STM32F0308DISCOVERY kit. My code is based on the ''UART_TwoBoards_ComIT'' example that I found in the STM32Cube repository (\STM32Cube\Repo...

how reach few uA current consumption in stm32f4 stop mode

Posted on October 07, 2014 at 15:24Hi,I’m working with an stm32f4xx mounted on Discovery platform; my goal is to measure current consumption in stop mode, using a multimeter (configured as amperometer) linked to the JP1 jumper. I use the UART2 to li...

DUrbano by Associate III
  • 3055 Views
  • 8 replies
  • 0 kudos

Recommeded for STM32F407 with DCMI

Posted on September 27, 2014 at 06:01I would like work easly and quickly camera with DCMI on STM32F407. Does anyone know sample source code on this system? I hope the program work parfect when I write to STM32 byEWARM. Actually, I already have a STM...

nagano by Associate II
  • 2525 Views
  • 7 replies
  • 0 kudos