STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem with STM32L0538 Discovery Board

Posted on October 09, 2014 at 14:30Hi guys,I just received the http://www.st.com/web/en/catalog/tools/FM116/SC959/SS1532/LN1848/PF260319?s_searchtype=keyword. When i connect it with computer, the E-Pager display some texts & images. Does any people ...

tien by Associate
  • 829 Views
  • 1 replies
  • 0 kudos

STM32f3 discovery, timer input capture problem

Posted on September 29, 2014 at 15:25 Hei, I'm sending a 3 us pulse to trigger the sensor. Than I have a time frame to reconfigure the pin in input capture, in order to measure the pulse. The pulse is working, but when I configurate the...

esovo1 by Associate II
  • 3101 Views
  • 12 replies
  • 0 kudos

MAC address for STM32F217

Posted on October 09, 2014 at 16:53guy,I am using STM32F217 for my product and there is Ethernet port in my product.  Since I need to do some pilot testing and I don't sure any MAC address built-in on the chip and then I can make use ST MAC address ...

hungli33 by Associate
  • 1774 Views
  • 3 replies
  • 0 kudos

Begineer questions

Posted on October 09, 2014 at 22:25Hi,I am just installed the STLink and Yagarto on my Mac OS 10.9.5 and it took me 3 days:( . I started the instance of STLINK by using command :./st-util --stlinkv1and after that I opened another terminal to run the...

sibagatu by Associate
  • 1206 Views
  • 2 replies
  • 0 kudos

SPI communication between two discovery Board

Posted on August 12, 2014 at 19:18Hello,        Can anyone help me with the an example of SPI communication between two STM32F4 Discovery Board. I have an example but with the HAL API which I dont want to use right now.RegardsSameer #stm32 #spi

STM32F0 (72) SPI 1 Wire Bidirectional with DMA BUG?

Posted on September 22, 2014 at 08:06Aim: Read 4 byte from MAX31855 (SPI readonly compatible) using SPI2  1wire bidirectional (using DMA) Code: (attached) Note:  SPI_CR1_BIDIMODE bit set  SO->MOSI  DMA   Channel4->RX   Channel5->TX (though garbage ...

Pointer Optimization

Posted on October 09, 2014 at 15:45Hi everyone, I'm working on an STM32F427 on a program with a huge linked list. I want to decrease the size of pointers used in this list in order to increase the number of elements in my ram. For instance, the memo...

benoit2 by Associate II
  • 1095 Views
  • 1 replies
  • 0 kudos

STM32F051R8 TMER3 ISSUE

Posted on September 22, 2014 at 16:48Hi.. In STM32F051R8 board, Iam using TIM3. I need to set timer interrupt for every every 10 seconds. Iam unable calculate the prescaler, CCR and time period values. Can any one explain me please...

stm32f4 discovery board is not working

Posted on October 09, 2014 at 08:47Hi everyoneI was working with stm32f4discovery board.It was working fine and i was able to execute my programs without any difficulties.Now after some day I am working with the same board.But my stm board is not ev...