cancel
Showing results for 
Search instead for 
Did you mean: 

Configuring SWCLK pin as an Input PullUp rather than the default Input PullDown

nicholas2399
Associate II
Posted on March 26, 2014 at 13:01

Hi all, your thoughts on this would be appreciated.

I have a need to re-configure the SWCLK pin on the STM32F103C8 (PA14) as an input with pull-up. By default on power up it is input puul-down. I still intend to use as SWCLK for my SW Debug.

I tried reprogramming the GPIOA_CRH and GPIOA_ODR registers to set this, but it had no affect on what the pin physically did.

As an experiment, I changed the MAPR to completely disable JTAG, thus release PA14. Now, changing GPIOA_CRH and GPIO_ODR correctly affects what the pin does.

OK, so I can accept that whilst the JTAG is enabled, that modifying the PulUp/PullDown status may not take affect, but what is strange is that if I:

Disable JTAG

Set PA14 as Pull Up

Re-enable JTAG

then the SWCLK pin retains the state I re-programmed it to.

Indeed after this sequence I can change the mode of the pin as I wish.

So taking this one step further i tried

Disable JTAG

Re-enable JTAG(SWD only)

Modify PA14 input mode

and this works as expected.

So it appears you have to disable jtag, then re-enable before you can modify the input mode of the pin.

This seems very odd does it not?

EDIT

Have now realised that disabling the JTAG pins then re-enabling the SWD pins doesn't work - it appears theat when I do this, the SWD interface is non functional (unless the SWD tries to communicate wilst NRST is active, which I cannot do). Almost as if once you turn the pins off, they remain off until reset!

Nick

#stm32f103-swd-swclk-afio-mapr
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0