Question
USB HID or CDC
Posted on March 12, 2014 at 11:01
Hi,
I have implemented the CDC(VCP) class on my F3 discovery and it work very well. Now, i want to send a integer data each 25µs. So i have to set up my rate speed of my board to 1600Kbps.On the PC side, the speed rate of my serial port is limited to 115Kbps.Is there any way to get the PC and the board working at the same speed 1600Kbps?Actually,i implemented HID class, my device is detected as HID device but i haven't tested the communication yet. I saw that the maximum speed is 64Kbytes/s. So, this solution can't resolve my problem.Do you have any idea how can i achieve this stuff ?I really need to use USB to communicate with my Board. Thanks in advance for any help,Best regards