STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Apparent bug in CubeMX clock generation

Posted on November 08, 2014 at 01:47 I seem to have found a bug in the clock configuration of the CubeMX software (Version 4.4.0, the latest as far as I can tell). On an STM32F407, I am setting the SYSCLK to use the PLL with the PLL source being...

mjones by Associate
  • 2530 Views
  • 2 replies
  • 0 kudos

STM32F429I SDRAM controller without byte select

Posted on November 08, 2014 at 05:37I waited for a 208 pin version for about a year and it is still not available (RUTRONIC now has 14 weeks wait time). So I want to try the STM32F429I (176 pins) for driving an RGB888 LCD with 32-bit SDRAM. It is ''...

michkhol by Associate
  • 1071 Views
  • 2 replies
  • 0 kudos

RM0091 documentation error (stm32f0x1/0x2/0x8)

Posted on November 07, 2014 at 13:03 Can you spot the (copy&paste) error in the following snippet from the stm32f0x1 reference manual ? If these MCUs are really capable of storing two bits in one, ST should probably file a patent...

Strange code behavior

Posted on November 07, 2014 at 23:09 I am working on project where i need to drive pjezo motors ( special triangle wave ) for generating forward or backward step i use timer controlled DMA , that copies triangle wave data to DAC output. ...

STM32F407VG+SRAM+ADDRESS PINS MISSING?

Posted on November 07, 2014 at 03:59I am trying to interface an external SRAM with the stm32f407vg discovery board and i bumped into some issues with address pins not being available for FSMC.As you guys might already know, the SRAM has both the Add...

0690X00000605UrQAI.png
mitjaneho by Associate II
  • 2768 Views
  • 6 replies
  • 0 kudos

STM32F4-discovery FreeRTOS

Posted on November 07, 2014 at 21:49Dear friends.I try to use freeRTOS on STM32F429I-DISCO. I want to create two tasks (blinking different leds) just to understand how the OS works. I use EWARM 7. When I compile the projects I have the following err...

baev_al by Associate III
  • 1329 Views
  • 3 replies
  • 0 kudos

STM32Cube USB Device Library dual DFU

Posted on November 06, 2014 at 09:07 Hello! I want to implement a dual DFU (Internal flash and SPI flash) on new STM32Cube USB Library. I've modified usbd_conf.h: /* DFU Class Config */ #define USBD_DFU_MAX_ITF_NUM 2 I've crea...

ivandevel by Associate II
  • 1386 Views
  • 1 replies
  • 1 kudos