STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F205zc ADC scan mode singel crosstalk problem

Posted on December 16, 2014 at 14:16I have a problem of crosstalk between sequence channels scan automaticly on the ADC3,2 of the MCU. It is look like it is depend on the sequnce of the sample becase the voltage changes on the first scan channel inf...

Barbie by Associate II
  • 1674 Views
  • 3 replies
  • 0 kudos

Doubt in Keil uVision

Posted on December 11, 2014 at 10:18Hello guys,I´m developing an application in Keil uVision and I am getting this message.What does this parameters mean?Program Size Code = ¿Flash?RO-Data = ¿?RW-Data = ¿?ZI-Data = ¿?

0690X00000603APQAY.jpg
gerardo by Associate II
  • 1717 Views
  • 3 replies
  • 0 kudos

PWM working but i can not change a pulse, STM32F3

Posted on December 15, 2014 at 17:19 Hello everybody, I've been working with my STM32 and to be honest I'm going to throw it out through my windows soon. I set a PWM (TIM1, CH1) and it actually was working preety well. Than I want to chang...

kajtek610 by Associate II
  • 1397 Views
  • 2 replies
  • 0 kudos

Confirming something about clocks

Posted on December 15, 2014 at 16:07Hello, I'm trying to confirm whether I understood the manual correctly.When setting up a clock's prescaler and counter, I should use the clock of the periphery bus it's connected to, right?, so for TIM4, with APB1...

jaravena by Associate
  • 1172 Views
  • 1 replies
  • 0 kudos

STM32F407 CAN Transmit doesn't work

Posted on December 15, 2014 at 17:13 Hello! I use STM32F407 Discovery board and want to use CAN1. My IDE is CoocoxIDE. I've putoscilloscopeon line PD1 (CAN TX) and haven't seen any activity...Discovery CAN works without any CAN IC (CAN Driver...

vasyl by Associate
  • 993 Views
  • 1 replies
  • 0 kudos

EXTI Problem with nucleo L152

Posted on December 14, 2014 at 14:21Hello,I've got a strange problem with setting an interrupt for input pins on my Nucleo board. Actualy, no one interrupt except EXTI15_10_IRQn doesn't work. I'm attaching two portions of code, one using input pin 1...

leosad by Associate II
  • 1865 Views
  • 3 replies
  • 0 kudos

DMA to external DAC transfer via SPI communication

Posted on November 13, 2014 at 13:32Hi everybody, I'm a beginner with STM32F30x µP. I'd like to made a DMA transfers from SRAM to an external DAC via SPI communication. Is it possible? Can I even configure a timer (TIMx) to generate a PWM signal or ...

franck2 by Associate II
  • 4128 Views
  • 19 replies
  • 0 kudos

no ir camera with stm32f4 discovery

Posted on December 15, 2014 at 00:08I want to use an infrared camera with stm32f4 discovery board. I thought in use a no ir raspberry pi camera, but I couldn't find any datasheet and pinout from this camera. Anyone know if I can use this camera with...

stm32nucleo legacy firmware

Posted on December 14, 2014 at 03:49Hi,I want to know where I can get the legacy libraries for stm32f401 nucleo boards (STM32 Nucleo_FW_VX.Y.Z) because I dont want to work with cube libraries.

gevides by Associate II
  • 1171 Views
  • 1 replies
  • 0 kudos